Hello,
I'm working with the "DVSDK_3_00_00_29" and the "SDK_1_0_2". My Hardware is the OMAP3EVM-Board and I'm using the original TI decode demo with the original video "davicieffect_ntsc_1.m4v" and "davicieffect_ntsc_1.264".
While playing the video the whole time you can see a few vertical and horizontal "stripes" on the lcd (see the attached pictures).
I think there is a problem with the TI codec. I talked about this topic whith TI a few times since December 2008 and according to TI the problem should be solved with the new "DVSDK_3_00_00_36" and the new "PSP-SDK-02.01.01.08". I tried it out but unfortunately the stripes are still there.
Has anyone seen this stripes too? Does anyone know how to solve this problem?
Best Regards.
Tino.