This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SGX driver for Android ICS beaglebone black

I'm using Android ICS on Beaglebone black kit. I'm replaced the kernel in Android ICS source and boot the device and i'm getting following errors in boot log

<6>[ 0.000000] AM335X ES2.0 (sgx neon )
<4>[ 0.000000] ------------[ cut here ]------------
<4>[ 0.000000] WARNING: at arch/arm/mach-omap2/clkt_clksel.c:194 omap2_clksel_recalc+0xc8/0xf8()
<4>[ 0.000000] clock: Could not find fieldval 0 for clock dpll_core_m6_ck parent dpll_core_x2_ck
<4>[ 0.000000] Modules linked in:
<4>[ 0.000000] Backtrace:
<4>[ 0.000000] [<c00189c0>] (dump_backtrace+0x0/0x114) from [<c05bdea0>] (dump_stack+0x20/0x24)
<4>[ 0.000000] r7:00000009 r6:000000c2 r5:c0031098 r4:c07f7e78
<4>[ 0.000000] [<c05bde80>] (dump_stack+0x0/0x24) from [<c0044558>] (warn_slowpath_common+0x5c/0x74)
<4>[ 0.000000] [<c00444fc>] (warn_slowpath_common+0x0/0x74) from [<c004462c>] (warn_slowpath_fmt+0x40/0x48)
<4>[ 0.000000] r9:c0bba840 r8:c089c190 r7:00000001 r6:00000002 r5:00000000
<4>[ 0.000000] r4:c080e6a8
<4>[ 0.000000] [<c00445ec>] (warn_slowpath_fmt+0x0/0x48) from [<c0031098>] (omap2_clksel_recalc+0xc8/0xf8)
<4>[ 0.000000] r3:00000000 r2:c06f1010
<4>[ 0.000000] [<c0030fd0>] (omap2_clksel_recalc+0x0/0xf8) from [<c0036458>] (propagate_rate+0x3c/0x5c)
<4>[ 0.000000] r7:c080037c r6:c089c1b8 r5:c080e5a8 r4:c080e6a8
<4>[ 0.000000] [<c003641c>] (propagate_rate+0x0/0x5c) from [<c0036464>] (propagate_rate+0x48/0x5c)
<4>[ 0.000000] r5:c080e54c r4:c080e594
<4>[ 0.000000] [<c003641c>] (propagate_rate+0x0/0x5c) from [<c0036464>] (propagate_rate+0x48/0x5c)
<4>[ 0.000000] r5:c080e494 r4:c080e538
<4>[ 0.000000] [<c003641c>] (propagate_rate+0x0/0x5c) from [<c0036464>] (propagate_rate+0x48/0x5c)
<4>[ 0.000000] r5:c080e380 r4:c080e480
<4>[ 0.000000] [<c003641c>] (propagate_rate+0x0/0x5c) from [<c00364c0>] (recalculate_root_clocks+0x48/0x60)
<4>[ 0.000000] r5:c081e540 r4:c080e36c
<4>[ 0.000000] [<c0036478>] (recalculate_root_clocks+0x0/0x60) from [<c07acbe8>] (am33xx_clk_init+0x88/0xa4)
<4>[ 0.000000] r5:c080e1fc r4:c080e1fc
<4>[ 0.000000] [<c07acb60>] (am33xx_clk_init+0x0/0xa4) from [<c07ac914>] (omap3xxx_clk_init+0xe0/0x32c)
<4>[ 0.000000] r5:80000200 r4:00003517
<4>[ 0.000000] [<c07ac834>] (omap3xxx_clk_init+0x0/0x32c) from [<c07a754c>] (am33xx_init_early+0x3c/0x40)
<4>[ 0.000000] r7:c080037c r6:c089c1b8 r5:80000200 r4:c07d17ec
<4>[ 0.000000] [<c07a7510>] (am33xx_init_early+0x0/0x40) from [<c07a3eac>] (setup_arch+0x72c/0x814)
<4>[ 0.000000] [<c07a3780>] (setup_arch+0x0/0x814) from [<c07a05ec>] (start_kernel+0x78/0x2e0)
<4>[ 0.000000] [<c07a0574>] (start_kernel+0x0/0x2e0) from [<80008040>] (0x80008040)
<4>[ 0.000000] r6:c07d2d2c r5:c07f8044 r4:10c53c7d
<4>[ 0.000000] ---[ end trace 1b75b31a2719ed1c ]---

<4>[ 7.636688] ------------[ cut here ]------------
<4>[ 7.641662] WARNING: at fs/sysfs/dir.c:481 sysfs_add_one+0x98/0xb8()
<4>[ 7.648498] sysfs: cannot create duplicate filename '/bus/platform/devices/pvrsrvkm'
<4>[ 7.656738] Modules linked in: pvrsrvkm(O+) wl12xx(O) mac80211(O) cfg80211(O) compat(O)
<4>[ 7.665313] Backtrace:
<4>[ 7.667968] [<c00189c0>] (dump_backtrace+0x0/0x114) from [<c05bdea0>] (dump_stack+0x20/0x24)
<4>[ 7.676971] r7:00000009 r6:000001e1 r5:c013a2f8 r4:ce253d30
<4>[ 7.683044] [<c05bde80>] (dump_stack+0x0/0x24) from [<c0044558>] (warn_slowpath_common+0x5c/0x74)
<4>[ 7.692565] [<c00444fc>] (warn_slowpath_common+0x0/0x74) from [<c004462c>] (warn_slowpath_fmt+0x40/0x48)
<4>[ 7.702636] r9:00003c23 r8:00000001 r7:ce278000 r6:ce277ef0 r5:ce278000
<4>[ 7.709625] r4:ffffffef
<4>[ 7.712463] [<c00445ec>] (warn_slowpath_fmt+0x0/0x48) from [<c013a2f8>] (sysfs_add_one+0x98/0xb8)
<4>[ 7.721893] r3:ce278000 r2:c07079a8
<4>[ 7.725738] [<c013a260>] (sysfs_add_one+0x0/0xb8) from [<c013b44c>] (sysfs_do_create_link+0x118/0x1f8)
<4>[ 7.735656] r7:cf013db0 r6:ce1d00e0 r5:ce253d88 r4:ce277ef0
<4>[ 7.741699] [<c013b334>] (sysfs_do_create_link+0x0/0x1f8) from [<c013b568>] (sysfs_create_link+0x1c/0x20)
<4>[ 7.751922] [<c013b54c>] (sysfs_create_link+0x0/0x20) from [<c02e357c>] (bus_add_device+0xd4/0x180)
<4>[ 7.761566] [<c02e34a8>] (bus_add_device+0x0/0x180) from [<c02e2124>] (device_add+0x478/0x598)
<4>[ 7.770721] r9:00003c23 r8:c08a8eb4 r7:c0840628 r6:00000000 r5:bf0fed00
<4>[ 7.777709] r4:bf0fecf8
<4>[ 7.780517] [<c02e1cac>] (device_add+0x0/0x598) from [<c02e6040>] (platform_device_add+0x108/0x1a4)
<4>[ 7.790161] [<c02e5f38>] (platform_device_add+0x0/0x1a4) from [<c02e610c>] (platform_device_register+0x30/0x34)
<4>[ 7.800903] r7:ce1095c0 r6:00000000 r5:bf0ff2f8 r4:bf0fecf0
<4>[ 7.807128] [<c02e60dc>] (platform_device_register+0x0/0x34) from [<bf10806c>] (init_module+0x6c/0x150 [pvrsrvkm])
<4>[ 7.818115] r5:bf0ff2f8 r4:00000000
<4>[ 7.822021] [<bf108000>] (init_module+0x0/0x150 [pvrsrvkm]) from [<c00086d8>] (do_one_initcall+0x4c/0x1ac)
<4>[ 7.832275] r6:00000000 r5:c0861c80 r4:bf0fefd0
<4>[ 7.837280] [<c000868c>] (do_one_initcall+0x0/0x1ac) from [<c007a020>] (sys_init_module+0x100/0x111c)
<4>[ 7.847106] [<c0079f20>] (sys_init_module+0x0/0x111c) from [<c00148a0>] (ret_fast_syscall+0x0/0x30)
<4>[ 7.856750] ---[ end trace 1b75b31a2719ed1e ]---
<4>[ 7.955444] omaplfb: Unknown symbol PVRGetDisplayClassJTable (err 0)

But i am using updated kernel i can see the updated patch in my kernel 

https://gitorious.org/rowboat/kernel/commit/d3ab5e87304b45dc594351ed091a6ae451f40de7?format=patch

and also i build the kernel wit PM_RUNTIME=1 by 

make TARGET_PRODUCT=am335xevm_sk OMAPES=4.x sgx PM_RUNTIME=1

but its not booting and here i've attached the dmesg. 

8054.SGX_BBB.txt