Hello,
In our application, we use the TMS320C674x for its calculation features only.
We use 1 SPI (boot loader) connected to an other microcontroller + the data bus (32 bits + 10 address) connected to an asynchronous SRAM, we don't use any other peripheral.
The external ambient temperature is around 90°C in our application.
What is happening on the DSP if the temperature increases ? Is there any disjonction or physical destruction ?
At a temperature below the potentiel disjonction or destruction, in our application, is there any modification of the performance in term of calculation feature (GFlop) ?
Thanks for your suppport.