This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MDC in EVM for OMAP3530

Hi,

I would like to know whether the MDC(Multimedia daughter card) that comes with EVM supports WinCE?

 

Regards,

Vicky

 

  • vicky said:
    I would like to know whether the MDC(Multimedia daughter card) that comes with EVM supports WinCE?

    I would probably look at this from the reverse context, that is rather does the WinCE BSP have support for video capture through the multimedia daughter card, which is something you may want to run past BSquare if you have not already as they own the WinCE BSP for the OMAP3. I believe there was some discussion on having this support a while back but I am not sure if it was ever implemented by BSquare.

  • Thanks for the reply,

    We are using LogicPD's BSP for WinCE. Bulk read is not working on the USB Host so we want to know whether the USB Host(particularly Bulk read and with WinCE) is working on the EVM or not.

    Regards,

    Vicky