This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

L137 Linux frame buffer question



Hi,

 

I'm using the Spectrum Digital L137 EVM with the DA830 UI board attached. The kernel (MontaVista) is configured to include fb and DA830/OMAP L137 display support. I'm running X by issuing "startx" as root. All is going fairly well - the Ice WM's taskbar seems to look a little truncated - but I don't want the LCD to blank after 10 minutes as it does. I've tried to running a short program to issue an ioctl command to kill blanking e.g. { ... ret_val = ioctl(fb_handle, FBIOBLANK, 0); ...} but get a return value of EINVAL no matter what.

 

Do I need to tweak the FB source to set blanking interval to 0, or have I (more likely) made a newbie mistake?

 

Thanks