This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[HW] DDR2 selection OMAP-L138/TMS320C6748

Hi all,

I'm new to this TI community, I hope to find here some TI experts and "collegue" to discuss commun problems :).

 

I'm looking for NON mobile DDR2 (extended temp range -40 +85C)  that may match the DDR2 controller (max 150Mhz clk).

At Micron Tech., for example , there aren't PN that run slowly ad 150Mhz. The, in production, devices run at minimum 333 Mhz with tck=3ns. I've not deep knowledge to this devices and I'd like to ask if for example the following PN MT47H32M16HR-3 IT can be used. I've supposed that using faster memory isn't a problem? Is that correct?

Correct me if I'm in wrong and, if possible, suggest me the correct "logic" or some links. I've read the Data sheets but there aren't information about this.

 

Thanks in advance.

MM