Other Parts Discussed in Thread: TMS320DM8168
Hi All,
The errata of TMS320DM8168 mentions to choose a NAND flash that is fully ONFI compatible.
Below are NAND flash from Micron:
1: MT29F2G16ABAEAWP-IT, which is 1.0 Compatible, 2Gb NAND
2: MT29F16G08ABABAWP-IT, which is 2.3 Compatible, 16Gb NAND
Is the DM8168 processor compatible with both the Nand Flash?
The DVR Ref Design about which Marc discusses in one of the forum questions is an 256*8 bit interface of Nand which is 1.0 compatible.
Regards,
Shah Kunal