This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Camera capture on omap35x evm

Hello,

I work on camera application with omap 35x evm platform and I would know how capture a stream preview from a camera device driver.

I've done a layered camera driver (to be usable by directshow) like the NULL camera driver or the camera_mdc driver ( the driver for the multimedia daughter card).

I select all item in directshow catalog.

I've done a subproject to test my driver :

CComPtr<IGraphBuilder> pGraph;

CComPtr<ICaptureGraphBuilder2> pBuild;

 HRESULT hr = CoInitialize(NULL);

if (SUCCEEDED(hr)){ 

   hr = CoCreateInstance(CLSID_FilterGraph, 0, CLSCTX_INPROC_SERVER,IID_IGraphBuilder, (void**)&pGraph);

   if (SUCCEEDED(hr)) {

        hr=CoCreateInstance(CLSID_CaptureGraphBuilder, NULL,CLSCTX_INPROC_SERVER, IID_ICaptureGraphBuilder2,(void**) &pBuild);

       if(SUCCEEDED(hr)){

            pBuild->SetFiltergraph(pGraph);

        }

        ... ... ...

I add in the source file :

WINCEATL80=1

INCLUDES= \

C:\WINCE600\PUBLIC\DIRECTX\SDK\INC; \

C:\WINCE600\OTHERS\ATL8\INCLUDE; \

$(_PROJECTROOT)\cesysgen\sdk\inc; \

TARGETLIBS= \

$(_PROJECTROOT)\cesysgen\sdk\lib\$(_CPUINDPATH)\ole32.lib \

$(_PROJECTROOT)\cesysgen\sdk\lib\$(_CPUINDPATH)\oleaut32.lib \

$(_PROJECTROOT)\cesysgen\sdk\lib\$(_CPUINDPATH)\uuid.lib \

$(_PROJECTROOT)\cesysgen\sdk\lib\$(_CPUINDPATH)\coredll.lib \

$(_PROJECTROOT)\cesysgen\sdk\lib\$(_CPUINDPATH)\Strmiids.lib \

$(_PROJECTROOT)\cesysgen\sdk\lib\$(_CPUINDPATH)\Strmbase.lib \

$(_PROJECTROOT)\cesysgen\sdk\lib\$(_CPUINDPATH)\dmoguids.lib \

C:\WINCE600\OTHERS\ATL8\LIB\ARMV4I\atls.lib \

C:\WINCE600\OTHERS\ATL8\LIB\ARMV4I\atlsd.lib \

Compilation, link OK but In the execution of my test : 

 hr=CoCreateInstance(CLSID_CaptureGraphBuilder, NULL,CLSCTX_INPROC_SERVER, IID_ICaptureGraphBuilder2,(void**) &pBuild);

Return always E_notImpl. Where is my error ? I'm use a bad lib ?

I would know how do you capture a stream from ISP camera if the problem come from the CaptureGraphBuilder2 object ? There is another method ?

 

Thanks you for your reply,

Baptiste D.

  • Ok, I found

    I rebuild my OSDesign with only the Multimedia daughter card sample and it's work.

    The problem come from my registry and the key

    [HKEY_LOCAL_MACHINE\Software\Microsoft\DirectX\DirectShow\Capture]

    That I've forgotten