Other Parts Discussed in Thread: UCD9081
Hi,
I am using UCD9081 in my hardware design. Since it is a slow device(max 100KHz), i couldn't able to write or read on the device since the UCD9081 requires clock stretching. (Refer: SLVS813A.pdf, page no. 9 - I2C Interface). I was using the same code for other high speed(400KHz) & low speed(100Hz) device, which doesn't have/required clock stretching. It was working fine for those.
My query is do we need to enable or configure any registers to enable clock stretching in OMAP I2C controller.
Kindly help me in this regards as soon as possible. We are blocked with this issue nearly for a month.
Regards,
V.Yuvaraj