When I use dvsdk_3_00_00_36, dvsdk_demos_3_00_00_11 decoder demo program to decode a video file from SD card on TI OMAP3EVM, I will receive an error message from console: "mmcblk0: retrying using single block read" and the demo program stopped. When I try to access the SD card from Linux shell, the whole system stopped. The funny thing is when I decode the video file from other location e,g, NFS, it works properly.
I need to get this to work with SD card because my project requires it.
Please help!