I have a customer who is wanting to use an AM335x device to take max 150Mb/s data in on USB and write out to a Gb Ethernet port. I've found some performance data here http://processors.wiki.ti.com/index.php/AM335x-PSP_04.06.00.08_Features_and_Performance_Guide#Ethernet_Driver. Looking at these metrics the bottleneck of the system appears to be the USB reads.
Although the bottleneck looks like USB reads the metrics are taken from read/writes to the peripherals and do not include memory transfers within the device. Is there a best practice for doing this? Can they use EDMA for memory transfers to avoid maxing out their CPU utilization? If so what are the performance penalties with respect to throughput?
I just want to make sure the bottleneck would in fact be the usb reads and not memory transfers within the device. Also by changing the CPU speed, will there be an increase in USB throughput? I believe in the TRM that the USB UTMI clock is fixed by the USB PHY to be 60MHz.
Thanks for the help,
Matt