This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

5509A Stops Executing Instructions

We’ve been working on a TI 5590A DSP-based design. After 3-4 days of continuous operation in a small loop the DSP stops executing instructions. All clock signals at the DSP are correct:

  1. Signal Name: OSCI, Desc: Osc input (11MHz XTAL Connection), PIN-13
  2. Signal Name: OSCO, Desc: output (11MHz XTAL Connection), PIN-14
  3. Signal Name: CLK, Desc:  44MHz Clock out, PIN-15

But the READ and WRITE lines are HIGH and not changing:

  1. Signal Name: AREN , Desc: Read Enable Strobe, PIN-16
  2. Signal Name: AWEN, Desc: Write Enable Strobe, PIN-19

The DSP goes to a Cyclone II PLD (Schematic attached). The PLD allows a reduced drive current mode. If we set the PLD to the reduced mode, then the MTBF is greatly improved but the problem still exists. We looked a BUS timings, power supply, etc. and didn’t find anything which would explain this issue. Has anyone seen a similar situation and what would be the next steps to investigate or resolve this?

Thanks,

Rich...

Schematic Page 5.pdf