Other Parts Discussed in Thread: TVP5147
Hi,
I'm using MISTRAL 8148 EVM board to testing LCD device,
it's worked fine in EZSDK framework, but when I run the same frame buffer testing program
in DVRRDK framework, I can't see anything from LCD and I sure that config
is correct like below info:
Fix Screen Info:
----------------
Line Length - 3200
Physical Address = 84e00000
Buffer Length = 3072000
Var Screen Info:
----------------
Xres - 800
Yres - 480
Xres Virtual - 800
Yres Virtual - 480
Bits Per Pixel - 32
Pixel Clk - 29850
Rotation - 0
Is there something wrong?
or is there any others example I can testing LCD in DVRRDK framework? thanks.