This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BeagleBone Black I2C max data rate?

HI, I have a BeagleBone Black card and I need to interface to another Processor through the I2C com port.

According to the data sheet on the AM335x CPU, the max speed is 400Kbps.

Is this a correct statement?

If the I2C ports are limited to 400Kbps, then I will need to use the SPI port.

Now, what is the fastest speed I can use the SPI ports at?

 

I need a minimum of 1mbps to transfer all of the pre-processed data to the BeagleBone Black module.

How can I do that reliably?