Hi
I am working with RDKDVR 4.0. TI816x. No HDMI Chip mod.
in file: ti_vsys.c
Int32 Vsys_create():
case VSYS_USECASE_MULTICHN_PROGRESSIVE_VCAP_VDIS_VENC_VDEC_4CH:
MultiCh_createProgressiveVcapVencVdecVdis();
When I run demo. There's exception:
Assertion @ Line: 100 in links_c6xdsp/alg_link/algLink_priv.c: pObj->
inQueInfo.numCh <= ALG_LINK_OSD_MAX_CH : failed !!!
Is i need add some init code in function:MultiCh_createProgressiveVcapVencVdecVdis();?
who can help me to do that?
Thanks.