This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can't boot after running the Re-flash Procedure - OMAP 35x EVM



Hi,

I was trying to re-flash with latest kernel, I operated as guided in the GettingStarted-02.01.01.08.pdf.  I did the re-flash several times because it  keep respond a "Kernel panic" error after reset.

But in my last trying, after I finished the *5.4.2 Running the Re-flash Procedure*, there's no more u-boot prompt on the TeraTerm or minicom anymore.

Before that I've re-flash the board with u-boot and uImage afforded in *OMAP35x-PSP-SDK-02.01.01.08*, it works good except errors like "kernel panic".

It is still able to re-flash u-boot through UART-3, but no help.

Also I failed to boot with SD. ( maybe need to set proper environment variable first?)

This board uses Micron Memory.

Pure newbie, need help.

Thanks,

Xi