Hi ,
My customer find that when set UART in RS485 mode(The default mode is RX), the TXD often transfer one more bit.
They compared UART status register 0x01D06014, when uart is ok, the reg value is 0x00->0x20->0x60. when in abnormal, the reg value is always 0x60.
Another finding is, the time between sending the TX cmd to uart and uart send out data is very long, which is obviously abnormal (baud rate 9600, 4Byte data, cost 100ms!)
Could you give some advice?
Thanks & Best regards,
Eason