Other Parts Discussed in Thread: OMAP3530
I have been trying to get the dynamic parameters working on the H.264 encoder, specifically the target bit rate.
But it does not seem to be working. The Max Bit Rate is working on creation of the encoder, but the target bit rate does not seem to have any affect on the video encoding process.
I am using the h264enc Codec supplied with dvsdk_3_00_00_29/omap3530_dvsdk_combos_3_16.
I am setting:
dynParams.targetBitRate to an integer value less than or equal to the MaxBiteRate
then calling:
VIDENC1_control( Venc1_getVisaHandle(hVe),
XDM_SETPARAMS,
(IVIDENC1_DynamicParams *)&device->dynParams,
&device->encStatus );
ret = Venc1_process(hVe, hInBuf, hOutBuf);
VIDENC1_control( Venc1_getVisaHandle(hVe),
XDM_GETSTATUS,
(IVIDENC1_DynamicParams *)&device->dynParams,
&device->encStatus );
but see no change in the encoded packet size/bit rate.
Can anyone confirm
1. My process is correct?
2. this feature is working with this version of the dvsdk/codec?
thanks for any help.