Other Parts Discussed in Thread: OMAP3530
We are facing an issue in configuring the gpio line 128 & 129 in OMAP3530 (Vers 3.0 & Vers 3.1) Chips. We couldn’t able to configure neither as output nor as input. We tested our code for other gpio lines present in our hardware & zoom kit, it is working fine.
Here with I am sending the code which we used to configure the lines as gpio output & tried to toggle the lines.
Kindly have a look & reply us as soon as possible. This is very urgent.
{
int result,iCount;
*(volatile unsigned int *)0x48005000 = 0x0003ffff; // GPIO2 -GPIO6 f clock
*(volatile unsigned int *)0x48005010 = 0x0003ffff; // GPIO2 -GPIO6 I clock
*(volatile unsigned int *)0x48004c00 |= 0x08; // GPIO1 f clock
*(volatile unsigned int *)0x48004c10 |= 0x08; // GPIO1 I clock
*(volatile unsigned int *)0x48002154 = 0x011c011c;// pad config for 128,129
*(volatile unsigned int *)0x49056034 &= 0xFFFFFFFC;// out put enable for 128,129
while(1)
{
*(volatile unsigned int *)0x4905603C |= 0x03;//
for(iCount=0;iCount<10000;iCount++);
*(volatile unsigned int *)0x4905603C &= ~0x03;//
for(iCount=0;iCount<10000;iCount++);
}
}