This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467 question about IPD(internal pulldown) on urxd2

HI,

we're using pin AB20 of DM6467 as UART2_RXD through pin-mux.

It can be used as uart, crg1_vcxi, gp or crg0_vcxi.

In addition, datasheet says its feature as IPD/DV_DD33 and I/O/Z.

then does it that it is internal PULL-DOWNed when we uses the AB20 pin as uart_rxd?

Is it impossible to disable internal pull-down through register configuration?

Thanks,

Devin