I'm trying to load a Windows CE image using the EVM Flash tool so that some of the guys working with the 3530 EVM board don't have to have Platform Builder installed, or mess with the SD loading method.
With previous WinCE eval products, I've loaded the NK.nb0 file directly into NAND without any issues. However, the EVM Flash tool doesn't allow downloading of .nb0 files. I found an option to convert nk.bin files into .raw format within the EVM Flash tool, but that didn't seem to load correctly. In looking at the memory map of the NAND, it appears as though the WinCE image binary gets loaded at 0x201C1800.
How do I get an NK file loaded into NAND using the TI EVM Flash application?
Thanks
dave