Hello.
I am considering to design using PCIe in C6657.
I have an question.
- Can I use 2lane PCIe separately as two port?
(I am gonna use both as endpoint.)
Best regards, RY
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
No, per PCIE user guide (SPRUGS6C—November 2012):
The PCI Express module supports the following features:
Supports a single bidirectional link interface (i.e., a single ingress port and a single egress port) with a maximum of two lanes width (×2)
The PCI Express module does not support the following features:
• No support for using ×2 link as two ×1 links
Regards, Eric