Other Parts Discussed in Thread: AM3517
Hi,
I'm trying to get the OMAP 35x EVM to boot off of a SD card and I'm not having any success.
I 've read and followed the very detailed post on this topic which began on 12/3/08.. I've dual-partitioned the SD card using fdisk as described in the instructions (several times), copied the MLO and uboot.bin from the SDK, and configured SW4 to what I *think* is correct. However, when I try to boot, although the SD card LED is lit, I get nothing out of the console.
My hardware setup:
- OMAP 3530 EVM (Mistral board?)
- 2GB ProMaster SD card (is this brand usable?)
- The settings for SW4 are SW4[8:1] = 11100110 (are these correct? also, are there any other jumpers I need to switch?)
My partitioning scheme:
One small (50M) bootable FAT32 partition (I've tried creating it with both fdisk and Windows: neither worked), and one ext3 partition. At the moment, I only have mlo and u-boot.bin on the SD card. I wanted to see x-loader start, then u-boot start - then the idea was I'd move on to adding the kernel and getting linux to boot.
Command (m for help): p
Disk /dev/sdd: 1967 MB, 1967128576 bytes
255 heads, 63 sectors/track, 239 cylinders
Units = cylinders of 16065 * 512 = 8225280 bytes
Device Boot Start End Blocks Id System
/dev/sdd1 * 1 7 56196 b W95 FAT32
/dev/sdd2 8 239 1863540 83 Linux
Command (m for help): x
Expert command (m for help): p
Disk /dev/sdd: 255 heads, 63 sectors, 239 cylinders
Nr AF Hd Sec Cyl Hd Sec Cyl Start Size ID
1 80 1 1 0 254 63 6 63 112392 0b
2 00 0 1 7 254 63 238 112455 3727080 83
3 00 0 0 0 0 0 0 0 0 00
4 00 0 0 0 0 0 0 0 0 00
Expert command (m for help):
user@laptop:~$ ls -l /media/sdcard/
total 120
-rwxr-xr-x 1 root root 8092 2008-12-31 09:04 mlo
-rwxr-xr-x 1 root root 109764 2008-12-31 09:04 u-boot.bin
Thanks.