Other Parts Discussed in Thread: OMAP3530
Hi,
I've been trying to gather some information about the OMAP Zoom2 development platform so that I can decide if the platform meets the needs of a graphics-intensive project I'm working on, but there are some areas which don't seem to be well documented. Could somebody please clarify:
- Is the "OMAP3430 SDK Linux v2.6 for Zoom" mentioned in [1] meant for this device? (I'm asking as there was/is also OMAP Zoom1.)
- If I get that SDK, can I use it with, say, Angstrom, to develop Linux Open GL ES applications? (Or anything else that is easily accessible. What I mean: Is that not too tightly bound to some specific distro/kernel?)
- Can I get the SDK before actually purchasing the device? (So that I can see what the SDK contains and can try to build something. I read the SDK page at TI website[1] says I just have to send a request by email. I did. But then I discovered a thread in this forum[2] which might imply I need to buy and register the kit first.)
- The kit contains a debug board. But I don't see any details about that either. Can this debug board be used with OpenOCD?
I searched through omapzoom.org, TI and logicpd.com webs and the web at large, but I couldn't find answers to those questions. I just feel like I did several loops following circular links. The closest thing I could find was [3], which has some answers, but it's about BeagleBoard, which is OMAP3530 based.
Thanks to anybody who can shed some light on this.
David
[1] http://focus.ti.com/general/docs/wtbu/wtbugencontent.tsp?templateId=6123&navigationId=12719&contentId=27458
[2] http://community.ti.com/forums/p/4028/14791.aspx#14791
[3] http://code.google.com/p/beagleboard/wiki/HowtoUseSGXunderAngstrom