This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

example of how to implement and use the Software Booting Configuration Structure in OMAP3530



Can someone offer some insights or point to an example in code (kernel or u-boot) regarding how software sets up the SW Booting Configuration Structure (as described in TRM 25.4.4.4)?  Particularly, must the structure itself be stored in a particular area in scratchpad memory?  Is the value at 0x48002910 supposed to be a pointer to the SW Booting Config Structure or the start of the structure itself?

Thanks.