Other Parts Discussed in Thread: SYSBIOS
Hi Everyone,
I am using concerto board and I am trying to add the I2C project into my project. When I added the below code into my I2C task function, I got the Exception occured problem. Can anyone help solve this?
Thanks in advance!
Bin
Code added:
transferOK = readEEPROM(Board_MPU6050_ADDRESS , ulRawData,
MPU6050_ADD_SIZE, MPU6050_DATA_SIZE);
if (!transferOK) {
System_abort("Error in I2C Transfer\n");
}
Console Message:
Update I2C
ti.sysbios.family.arm.m3.Hwi: line 938: E_hardFault: FORCED
ti.sysbios.family.arm.m3.Hwi: line 1015: E_busFault: PRECISERR: Immediate Bus Fault, exact addr known, address: fdbfffff
Exception occurred in background thread at PC = 0x0021fed8.
Core 0: Exception occurred in ThreadType_Task.
Task name: task1, handle: 0x200104e4.
Task stack base: 0x2000c7a0.
Task stack size: 0x800.
R0 = 0x3a97e7ff R8 = 0x0022ab28
R1 = 0x20010aa0 R9 = 0x1d880300
R2 = 0x00000002 R10 = 0x00000001
R3 = 0xfdbfffef R11 = 0x00000020
R4 = 0x200104e4 R12 = 0x0022ab20
R5 = 0x20010294 SP(R13) = 0x2000e6f0
R6 = 0x20010aa0 LR(R14) = 0x0021fecb
R7 = 0x00000000 PC(R15) = 0x0021fed8
PSR = 0x01000200
ICSR = 0x00423803
MMFSR = 0x00
BFSR = 0x82
UFSR = 0x0000
HFSR = 0x40000000
DFSR = 0x00000000
MMAR = 0xfdbfffff
BFAR = 0xfdbfffff
AFSR = 0x00000000
Terminating execution...