Other Parts Discussed in Thread: AM3517, AM3358
how to install VNC on Zoom™ AM3517 eXperimenter Kit arago-project linux??
i try "opkg install x11vnc" but doesn´t work
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I believe the Arago feeds have been removed some time ago since they hadn't been updated. Check this post out.
Maybe you can use the Angstrom base feed instead: feeds.angstrom-distribution.org
http://www.angstrom-distribution.org/repo/?section=base
Check this forum topic: http://e2e.ti.com/support/arm/sitara_arm/f/791/p/266848/934991.aspx#934991 where I have pointed out how to add a package feed source to your opkg configuration.
Best regards,
Miroslav
You can always cross compile it.
Download the x11vnc source code from here: http://www.karlrunge.com/x11vnc/
There is a pretty good explanation on how to cross compile it inside the README file:
Q-118: How do I cross compile x11vnc for a different architecture than
my Linux i386 or amd64 PC?
You will need a cross-compiling toolchain. Perhaps your distro
provides these or you can find a HOWTO for your distro. We found a
nice one at qtmoko.org for building armel binaries on Debian Linux
i386 machines. It includes most of the libraries that x11vnc needs. We
use that example here.
We ran this script to set PATH, configure, and build:
#!/bin/sh
# toolchain from: qtmoko-debian-toolchain-armv4t-eabi.tar.gz
export PATH=/opt/toolchains/arm920t-eabi/bin:$PATH
env CC=arm-linux-gcc ./configure --host=arm-linux --without-avahi
make
arm-linux-strip ./x11vnc/x11vnc
ls -l ./x11vnc/x11vnc
Note we had to include --without-avahi due to lack of
libavahi-client.so.3 supplied by the toolchain we used. One would need
to add it if it was desired on the target machine. We also stripped
the binary to make it smaller.
For an embedded system one may also want to add --without-x if the
embedded system does not use X11 and the -rawfb mechanism must be
used.
Of course you need to specify the gcc cross compiler path and name from the SDK you are using.
Best regards,
Miroslav
Hello Miroslav and everybody
I use ti-sdk-am335x-evm-06.00.00.00 and I have cross compiled x11vnc-0.9.13 so:
source ../ti-sdk-am335x-evm-06.00.00.00/linux-devkit/environment-setup
./configure --host=arm-linux-gnueabihf --without-avahi --without-x --without-filetransfer --without-crypt --without-crypto --without-ssl
make
I can run x11vnc on AM3358 but I does not find X buffer and it does not work:
root@am335x-evm:~/vnc# ./x11vnc
###############################################################
#@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@#
#@ @#
#@ ** WARNING ** WARNING ** WARNING ** WARNING ** @#
#@ @#
#@ YOU ARE RUNNING X11VNC WITHOUT A PASSWORD!! @#
#@ @#
#@ This means anyone with network access to this computer @#
#@ may be able to view and control your desktop. @#
#@ @#
#@ >>> If you did not mean to do this Press CTRL-C now!! <<< @#
#@ @#
#@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@#
#@ @#
#@ You can create an x11vnc password file by running: @#
#@ @#
#@ x11vnc -storepasswd password /path/to/passfile @#
#@ or x11vnc -storepasswd /path/to/passfile @#
#@ or x11vnc -storepasswd @#
#@ @#
#@ (the last one will use ~/.vnc/passwd) @#
#@ @#
#@ and then starting x11vnc via: @#
#@ @#
#@ x11vnc -rfbauth /path/to/passfile @#
#@ @#
#@ an existing ~/.vnc/passwd file from another VNC @#
#@ application will work fine too. @#
#@ @#
#@ You can also use the -passwdfile or -passwd options. @#
#@ (note -passwd is unsafe if local users are not trusted) @#
#@ @#
#@ Make sure any -rfbauth and -passwdfile password files @#
#@ cannot be read by untrusted users. @#
#@ @#
#@ Use x11vnc -usepw to automatically use your @#
#@ ~/.vnc/passwd or ~/.vnc/passwdfile password files. @#
#@ (and prompt you to create ~/.vnc/passwd if neither @#
#@ file exists.) Under -usepw, x11vnc will exit if it @#
#@ cannot find a password to use. @#
#@ @#
#@ @#
#@ Even with a password, the subsequent VNC traffic is @#
#@ sent in the clear. Consider tunnelling via ssh(1): @#
#@ @#
#@ http://www.karlrunge.com/x11vnc/#tunnelling @#
#@ @#
#@ Or using the x11vnc SSL options: -ssl and -stunnel @#
#@ @#
#@ Please Read the documention for more info about @#
#@ passwords, security, and encryption. @#
#@ @#
#@ http://www.karlrunge.com/x11vnc/faq.html#faq-passwd @#
#@ @#
#@ To disable this warning use the -nopw option, or put @#
#@ 'nopw' on a line in your ~/.x11vncrc file. @#
#@ @#
#@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@@#
###############################################################
28/06/2013 15:28:05 x11vnc version: 0.9.13 lastmod: 2011-08-10 pid: 1664
28/06/2013 15:28:05 This x11vnc was built without X11 support (-rawfb only).
28/06/2013 15:28:05
28/06/2013 15:28:05 *** XOpenDisplay failed. No -display or DISPLAY.
28/06/2013 15:28:05 *** Trying ":0" in 4 seconds. Press Ctrl-C to abort.
28/06/2013 15:28:05 *** 1 2 3 4
28/06/2013 15:28:09 This x11vnc was built without X11 support (-rawfb only).
28/06/2013 15:28:09
28/06/2013 15:28:09 ***************************************
28/06/2013 15:28:09 *** XOpenDisplay failed (:0)
*** x11vnc was unable to open the X DISPLAY: ":0", it cannot continue.
*** There may be "Xlib:" error messages above with details about the failure.
Some tips and guidelines:
** An X server (the one you wish to view) must be running before x11vnc is
started: x11vnc does not start the X server. (however, see the -create
option if that is what you really want).
** You must use -display <disp>, -OR- set and export your $DISPLAY
environment variable to refer to the display of the desired X server.
- Usually the display is simply ":0" (in fact x11vnc uses this if you forget
to specify it), but in some multi-user situations it could be ":1", ":2",
or even ":137". Ask your administrator or a guru if you are having
difficulty determining what your X DISPLAY is.
** Next, you need to have sufficient permissions (Xauthority)
to connect to the X DISPLAY. Here are some Tips:
- Often, you just need to run x11vnc as the user logged into the X session.
So make sure to be that user when you type x11vnc.
- Being root is usually not enough because the incorrect MIT-MAGIC-COOKIE
file may be accessed. The cookie file contains the secret key that
allows x11vnc to connect to the desired X DISPLAY.
- You can explicitly indicate which MIT-MAGIC-COOKIE file should be used
by the -auth option, e.g.:
x11vnc -auth /home/someuser/.Xauthority -display :0
x11vnc -auth /tmp/.gdmzndVlR -display :0
you must have read permission for the auth file.
See also '-auth guess' and '-findauth' discussed below.
** If NO ONE is logged into an X session yet, but there is a greeter login
program like "gdm", "kdm", "xdm", or "dtlogin" running, you will need
to find and use the raw display manager MIT-MAGIC-COOKIE file.
Some examples for various display managers:
gdm: -auth /var/gdm/:0.Xauth
-auth /var/lib/gdm/:0.Xauth
kdm: -auth /var/lib/kdm/A:0-crWk72
-auth /var/run/xauth/A:0-crWk72
xdm: -auth /var/lib/xdm/authdir/authfiles/A:0-XQvaJk
dtlogin: -auth /var/dt/A:0-UgaaXa
Sometimes the command "ps wwwwaux | grep auth" can reveal the file location.
Starting with x11vnc 0.9.9 you can have it try to guess by using:
-auth guess
(see also the x11vnc -findauth option.)
Only root will have read permission for the file, and so x11vnc must be run
as root (or copy it). The random characters in the filenames will of course
change and the directory the cookie file resides in is system dependent.
See also: http://www.karlrunge.com/x11vnc/faq.html
When I remove "--without-x" option it does not compile:
========================================================================== *** A working X window system build environment is required to build *** x11vnc. Make sure any required X development packages are installed. If they are installed in non-standard locations, one can use the --x-includes=DIR and --x-libraries=DIR configure options or set the CPPFLAGS and LDFLAGS environment variables to indicate where the X window system header files and libraries may be found. On 64+32 bit machines you may need to point to lib64 or lib32 directories to pick up the correct word size. If you want to build x11vnc without X support (e.g. for -rawfb use only or for native Mac OS X), specify the --without-x configure option. ==========================================================================
How can I get VNC working in AM335x EVM?
And what command do you use to run the VNC server?
Best regards,
Miroslav
I have tried:
root@am335x-evm:~/vnc# ./x11vnc
root@am335x-evm:~/vnc# ./x11vnc -display :0
root@am335x-evm:~/vnc# ./x11vnc -display /dev/fb0
root@am335x-evm:~/vnc# ./x11vnc -display /dev/fb
I execute it by hand from uart0 terminal.
Does ti-sdk-am335x-evm-06.00.00.00 include X11?. Maybe x11vnc is not the best vnc server or whatever software that allows me to control AM335x EVM with a broken touchscreen from my computer .
Best regards
Have you compiled and installed the Graphics SDK with X11 support?
Best regards,
Miroslav
No, I haven't, I use the root filesystem /home/sitara/ti-sdk-am335x-evm-06.00.00.00/targetNFS, maybe it is already installed.
lsmod returns 0 modules, so I think it is not installed.
My custom Qt aplication runs fine, should I install Graphics SDK for vnc?, is there any other simmilar software? (remote control)
Best regards
I think it is included in the larger root file system, but it's pre-compiled with SUPPORT_XORG=0, so you will need to follow the instructions here and compile it with Xorg support, then install it into your targetfs.
Best regards,
Miroslav
P.S. Please check this post by Josh Elliott: http://e2e.ti.com/support/arm/sitara_arm/f/791/p/314332/1094502.aspx#1094502