Other Parts Discussed in Thread: DM385
Hello,
My customer is desiging interface circuit between DM385 processor and Sony IMX172 image sensor using SN65LVDS324. The reference circuit on the datasheet of SN65LVDS324 shows an example using IMX136. However, it seems that IMX136's HSYNC / VSYNC pin is opened. This means that there is no input signal for HSYNC / VSYNC of image sensor. SN65LVDS324 generate HSYNC / VSYNC only for processor. Is it possible that image sensor can generate data signal without receiving any HSYNC / VSYNC signal ? I think TI's SN65LVDS324 reference circuit is designed based on no HSYNC / VSYNC signal into image sensor.Sony told that the image sensor IMX172 they are about to use only provide slave mode (HSYNC, VSYNC input) and it doesn't work without HSYNC / VSYNC input
Best wishes
Carter