Hello everyone,
I added the following statements to MemorySetup() function in C:\WINCE600\PLATFORM\SUN35x\SRC\BOOT\XLDR\platform.c
OUTREG32(&pGpmc->GPMC_CONFIG1_3, BSP_GPMC_CONFIG1);
#define BSP_GPMC_CONFIG1 0x29801201;
#define BSP_GPMC_CONFIG2 0x00111102;
#define BSP_GPMC_CONFIG3 0x00070703;
#define BSP_GPMC_CONFIG4 0x10091009;
#define BSP_GPMC_CONFIG5 0x010E1111;
#define BSP_GPMC_CONFIG6 0x0A080000;
#define BSP_GPMC_CONFIG7 0x00000858;
Then I flashed the newly built XLDRNAND.nb0 to the nand flash through the serial port, but it failed. The screen sayed
"ERROR: OEMWriteFlash: XLDR image must have only one module and no file