I am working with the McBSP channels on the OMAP35xx EVM and I am having some issues or perhaps misunderstanding of McBSP 1. I have sucessfully implemented output on McBSP1 and can do input on channels 2 and 3 and even have DMA working.
The question is. Can one do bidirectional communications on McBSP1 simultaneously/concurrely? Since device 1 brings out so many signals, it would seem logical that this is possible. However, I have to first get input to work by itself. When I use the register configuration that works on the other channels there is still no luck.
Any ideas would be greatly appreciated.