Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Configuring the PLL in SYS/BIOS

Other Parts Discussed in Thread: SYSBIOS

I have been migrating a project from DSP/BIOS to SYS/BIOS for the 28335 and have run into another question.  In the legacy code, there is a call within main at the beginning of the code to a user init code that configures the PLL.

I'm battling an issue where my application never reaches the breakpoint at main() and when I let the program run and halt it, I often halt it when it is in the middle of this code, so I'm wondering if it is the culprit. In this function is the following:

//--- Configure the PLL

// Note: The DSP/BIOS configuration tool can also be used to initialize the PLL
// instead of doing the initialization here.

 // Make sure the PLL is not running in limp mode
 if (SysCtrlRegs.PLLSTS.bit.MCLKSTS != 1)
 {             // PLL is not running in limp mode
  SysCtrlRegs.PLLSTS.bit.MCLKOFF = 1;    // Turn off missing clock detect before changing PLLCR
  SysCtrlRegs.PLLSTS.bit.DIVSEL = 0;    // DIVSEL must be 0 or 1  (/4 CLKIN mode) before changing PLLCR
  SysCtrlRegs.PLLCR.bit.DIV = 0x000A;    // PLLx10/4 (because DIVSEL is /4)
  
  // Wait for PLL to lock.
  // During this time the CPU will run at OSCCLK/2 until the PLL is stable.
  // Once the PLL is stable the CPU will automatically switch to the new PLL value.
  // Code is not required to sit and wait for the PLL to lock.  However,
  // if the code does anything that is timing critical (e.g. something that
  // relies on the CPU clock frequency to be at speed), then it is best to wait
  // until PLL lock is complete.  The watchdog should be disabled before this loop
  // (e.g., as was done above), or fed within the loop.
  while(SysCtrlRegs.PLLSTS.bit.PLLLOCKS != 1)  // Wait for PLLLOCKS bit to set
  {
   SysCtrlRegs.WDKEY = 0x0055;     // Service the watchdog while waiting
   SysCtrlRegs.WDKEY = 0x00AA;     //   in case the user enabled it.
  }

  // After the PLL has locked, we are running in PLLx10/4 mode (since DIVSEL is /4).
  // We can now enable the missing clock detect circuitry, and also change DIVSEL
  // to /2.  In this example, we will wait a bit of time to let inrush currents settle,
  // and then change DIVSEL from /4 to /2.  This is only an example.  The amount of
  // time you need to wait depends on the power supply feeding the DSP (i.e., how much
  // voltage droop occurs due to the inrush currents, and how long it takes the
  // voltage regulators to recover).
  SysCtrlRegs.PLLSTS.bit.MCLKOFF = 0;    // Enable missing clock detect circuitry
  DelayUs(20/2);         // Wait 20 us (just an example).  Remember we're running
              // at half-speed here, so divide function argument by 2.
  SysCtrlRegs.PLLSTS.bit.DIVSEL = 0x2;   // Change to /2 mode
 }
 else
 {             // PLL is running in limp mode
 // User should replace the below with a call to an appropriate function,
 // for example shutdown the system (since something is very wrong!).
  Reset();
 }

I attemped to have SYS/BIOS configure the PLL by checking the box in the boot section of the cfg file.  I commented out the above code, and checked the box and tried to build.  Naturally it failed to build and gave this error:

error: ti.sysbios.BIOS: "C:/ti/bios_6_34_04_22/packages/ti/sysbios/BIOS.xs", line 209: ti.sysbios.BIOS : BIOS.cpuFreq is undefined.  You must define the CPU frequency in your application configuration.  For example, if the PLL is being configured for 100MHz, add this to your application configuration script: BIOS.cpuFreq.lo = 100000000;
js: "C:/ti/xdctools_3_25_02_70/packages/xdc/cfg/Main.xs", line 153: Error: Configuration failed!
gmake.exe: *** [package/cfg/Semikron_DCDC_v05_p28FP.xdl] Error 1
js: "C:/ti/xdctools_3_25_02_70/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake: Target `all' not remade because of errors.

When I add:

BIOS.cpuFreq.lo = 10000000;

to the cfg script, the error remains.  If I change it to:

BIOS.cpuFreq = 10;

I recieve this error:

configuring Semikron_DCDC_v05.x28FP from package/cfg/Semikron_DCDC_v05_p28FP.cfg ...
js: "C:/Users/Admin/Desktop/Semikron_SYSBIOS/Semikron_SYSBIOS/Semikron_DCDC_v05.cfg", line 564: XDC runtime error: ti.sysbios.BIOS/cpuFreq: incompatible assignment: 10.0
    "./package/cfg/Semikron_DCDC_v05_p28FP.cfg", line 177
gmake.exe: *** [package/cfg/Semikron_DCDC_v05_p28FP.xdl] Error 1
js: "C:/ti/xdctools_3_25_02_70/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake: Target `all' not remade because of errors.

 

 I guess my questions are:

 Is the above code the correct method for configuring the PLL for SYS?BIOS? 

Am I doing something wrong in trying to configure the PLL through the cfg file?

  • Hi Justin,

    The correct method (and easiest) is to use the cfg file to configure the PLL.  There is something very odd about with your screenshot.  I created an example and added the PLL configuration.  The Frequency field was automatically set to 50 MHz.  Can you verify that all of the aforementioned code has been removed?  Additionally, can you post your cfg file?

    Thanks,

    -- Emmnauel