This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

x-loader + lauterbach on OMAP3430



Hi,

I am trying to get Linux on an OMAP-based board developed inhouse, and immediately ran into a problem when trying to get the boot steps x-loader+u-boot into place.

I have adapted them and can run both of them via Lauterbach, but I am having a problem with one line in the x-loader code that I don't really understand. I have taken x-loader from the omapzoom wiki, and figured it should be easy enough to run this on our board.

However, when I step through the initial code in the x-loader using Lauterbach the program always crashes in the same place. In the routine cpu_init_crit in cpu/omap3/start.S there is a cryptical statement which makes the processor crash every time I pass it:

----------------------------------------------------------------------------------------

 cpu_init_crit:
        /*
         * Invalidate L1 I/D
         */
        mov     r0, #0                 /* set up for MCR */
        mcr     p15, 0, r0, c8, c7, 0  /* invalidate TLBs */
        mcr     p15, 0, r0, c7, c5, 1  /* invalidate icache */

        /* Invalide L2 cache (gp device call point)
         * - warning, this may have issues on EMU/HS devices
         * this call can corrupt r0-r5
         */
        mov r12, #0x1           @ set up to invalide L2
smi:    .word 0xE1600070        @ Call SMI monitor                       <---- Crash statement


        /*
         * disable MMU stuff and caches
         */
----------------------------------------------------------------------------------------

As I understand this statement it has something to do with L2-cache. If I skip this statement in Lauterbach the rest of the loader runs fine.

Does anyone have any idea why this crashes for me? My CPU is a OMAP3430 ES2.0.

Could this be related to Lauterbach only? I was planning to boot from SD card but haven't been able to try these steps out yet.

Thanks!

-Magnus