HI,
I am using the kernel from git clone git://git.omapzoom.org/kernel/omap.git kernel/android-3.4 which is provided in http://omapedia.org/wiki/Panda5AJ.1.5_Release_Notes.
I need to enable hardware acceleration for Graphics and Multimedia kernel drivers. With the prebuild binaries we are able to get the playback H.264 video on Panda board.
But to build against our custom kernel I need to get the source code of the omapdce driver. which is not present in the kernel tree.
From where I can get the matching omapdce driver source code compatible with Panda5AJ.1.5 kenel ?
From where i can obtain the userspace source code for Panda5AJ.1.5 to get hardware acceleration working
Reference hardware platform used : TI OMAP5 5432 uEVM ES2.0 (Panda5)
Regards,
IShaqe