Hi All,
I am working to run openGLES 3D application on Beaglebone+DVID cape using SGX driver. After doing many trial with multiple linux kernel sources(psp) available in web, I ended-up with running only few basic unittests. But 3D am unable to run . This is because i assume most of these linux BSP available is less compatible for openGLES. Even after reading some e2e posts i found TI-SDK having support for openGLES 3D(glxgears). But when am trying to boot my Beaglebone+DVID cape with "ti-sdk-am335x-evm-05.07.00.00-linux-X86-install" i ended with no display and /dev/fb0 (This can observe attached file
U-Boot SPL 2013.01.01 (Apr 04 2013 - 23:46:57)                                                   
No AC power, disabling frequency switch                                                          
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0                                             
musb-hdrc: setup fifo_mode 4            
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0        
musb-hdrc: setup fifo_mode 4            
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
OMAP SD/MMC: 0
reading u-boot.img
reading u-boot.img
U-Boot 2013.01.01 (Apr 04 2013 - 23:46:57)
I2C:   ready
DRAM:  256 MiB
WARNING: Caches not enabled
NAND:  No NAND device found!!!
0 MiB
MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - readenv() failed, using default environment
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0 
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0 
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
Net:   <ethaddr> not set. Validating first E-fuse MAC
cpsw, usb_ether
Hit any key to stop autoboot:  0 
mmc0 is current device
SD/MMC found on device 0
reading uEnv.txt
** Unable to read file uEnv.txt **
reading uImage
3286864 bytes read in 403 ms (7.8 MiB/s)
Booting from mmc ...
## Booting kernel from Legacy Image at 80007fc0 ...
   Image Name:   Linux-3.2.0
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    3286800 Bytes = 3.1 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   XIP Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[    0.000000] Linux version 3.2.0 (root@igx-desktop) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #3 Tue Oct 22 21:29:48 IST 2013
[    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine: am335xevm
[    0.000000] Memory policy: ECC disabled, Data cache writeback
[    0.000000] AM335X ES1.0 (sgx neon )
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 65024
[    0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext3 rootwait ip=none
[    0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[    0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[    0.000000] Memory: 256MB = 256MB total
[    0.000000] Memory: 252940k/252940k available, 9204k reserved, 0K highmem
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xd0800000 - 0xff000000   ( 744 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)
[    0.000000]     modules : 0xbf000000 - 0xc0000000   (  16 MB)
[    0.000000]       .text : 0xc0008000 - 0xc05ea000   (6024 kB)
[    0.000000]       .init : 0xc05ea000 - 0xc0626000   ( 240 kB)
[    0.000000]       .data : 0xc0626000 - 0xc06904a0   ( 426 kB)
[    0.000000]        .bss : 0xc06904c4 - 0xc06c07e4   ( 193 kB)
[    0.000000] NR_IRQS:396
[    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[    0.000000] Total of 128 interrupts on 1 active controller
[    0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[    0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[    0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[    0.000000] Console: colour dummy device 80x30
[    0.000183] Calibrating delay loop... 548.86 BogoMIPS (lpj=2744320)
[    0.048339] pid_max: default: 32768 minimum: 301
[    0.048461] Security Framework initialized
[    0.048583] Mount-cache hash table entries: 512
[    0.049041] CPU: Testing write buffer coherency: ok
[    0.070739] omap_hwmod: pruss: failed to hardreset
[    0.072326] print_constraints: dummy: 
[    0.072753] NET: Registered protocol family 16
[    0.075439] OMAP GPIO hardware version 0.1
[    0.078765] omap_mux_init: Add partition: #1: core, flags: 0
[    0.081237]  omap_i2c.1: alias fck already exists
[    0.082336]  omap2_mcspi.1: alias fck already exists
[    0.082611]  omap2_mcspi.2: alias fck already exists
[    0.083801]  edma.0: alias fck already exists
[    0.083831]  edma.0: alias fck already exists
[    0.083862]  edma.0: alias fck already exists
[    0.119415] bio: create slab <bio-0> at 0
[    0.122161] SCSI subsystem initialized
[    0.124176] usbcore: registered new interface driver usbfs
[    0.124572] usbcore: registered new interface driver hub
[    0.124816] usbcore: registered new device driver usb
[    0.125000] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[    0.125366] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[    0.138336] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[    0.140136] tps65910 1-002d: could not be detected
[    0.141815] Advanced Linux Sound Architecture Driver Version 1.0.24.
[    0.143218] Switching to clocksource gp timer
[    0.163452] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[    0.163665] musb-hdrc musb-hdrc.0: dma type: pio
[    0.164062] MUSB0 controller's USBSS revision = 4ea20800
[    0.164916] musb-hdrc musb-hdrc.0: USB OTG mode controller at d083c000 using PIO, IRQ 18
[    0.165130] musb-hdrc musb-hdrc.1: dma type: pio
[    0.165496] MUSB1 controller's USBSS revision = 4ea20800
[    0.165740] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[    0.165832] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[    0.165985] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[    0.166015] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    0.166015] usb usb1: Product: MUSB HDRC host driver
[    0.166046] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd
[    0.166046] usb usb1: SerialNumber: musb-hdrc.1
[    0.167114] hub 1-0:1.0: USB hub found
[    0.167175] hub 1-0:1.0: 1 port detected
[    0.167816] musb-hdrc musb-hdrc.1: USB Host mode controller at d083e800 using PIO, IRQ 19
[    0.168334] NET: Registered protocol family 2
[    0.168548] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.168914] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[    0.169097] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[    0.169219] TCP: Hash tables configured (established 8192 bind 8192)
[    0.169250] TCP reno registered
[    0.169281] UDP hash table entries: 256 (order: 0, 4096 bytes)
[    0.169311] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[    0.169525] NET: Registered protocol family 1
[    0.169830] RPC: Registered named UNIX socket transport module.
[    0.169860] RPC: Registered udp transport module.
[    0.169860] RPC: Registered tcp transport module.
[    0.169891] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.170166] NetWinder Floating Point Emulator V0.97 (double precision)
[    0.183105] VFS: Disk quotas dquot_6.5.2
[    0.183197] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.183959] msgmni has been set to 494
[    0.187866] alg: No test for stdrng (krng)
[    0.188629] io scheduler noop registered
[    0.188659] io scheduler deadline registered
[    0.188720] io scheduler cfq registered (default)
[    0.190307] Could not set LED4 to fully on
[    0.192535] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[    0.742065] console [ttyO0] enabled
[    0.746459] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[    0.754425] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[    0.762268] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[    0.770202] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[    0.778106] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[    0.786621] omap4_rng omap4_rng: OMAP4 Random Number Generator ver. 2.00
[    0.805847] brd: module loaded
[    0.815612] loop: module loaded
[    0.819122] i2c-core: driver [tsl2550] using legacy suspend method
[    0.825653] i2c-core: driver [tsl2550] using legacy resume method
[    0.832092] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[    0.893768] No daughter card found
[    0.897369] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[    0.912597] Board name: A335BONE
[    0.916015] Board version: 00A6
[    0.919281] The board is a AM335x Beaglebone.
[    0.926330] tps65217 1-0024: TPS65217 ID 0xf version 1.2
[    0.934173] print_constraints: DCDC1: 900 <--> 1800 mV at 1800 mV 
[    0.942901] print_constraints: DCDC2: 900 <--> 3300 mV at 1275 mV 
[    0.951660] print_constraints: DCDC3: 900 <--> 1500 mV at 1100 mV 
[    0.960327] print_constraints: LDO1: 1000 <--> 3300 mV at 1800 mV 
[    0.967071] usb 1-1: new high-speed USB device number 2 using musb-hdrc
[    0.976348] print_constraints: LDO2: 900 <--> 3300 mV at 3300 mV 
[    0.984985] print_constraints: LDO3: 1800 <--> 3300 mV at 3300 mV 
[    0.993713] print_constraints: LDO4: 1800 <--> 3300 mV at 3300 mV 
[    1.000732] Maximum current provided by the USB port is 500mA which is not sufficient
[    1.000762] when operating @OPP120 and OPPTURBO. The current requirement for some
[    1.000762] use-cases using OPP100 might also exceed the maximum current that the
[    1.000793] USB port can provide. Unless you are fully confident that the current
[    1.000793] requirements for OPP100 use-case don't exceed the USB limits, switching
[    1.000793] to AC power is recommended.
[    1.045013]  omap_hsmmc.0: alias fck already exists
[    1.050689]  omap_i2c.3: alias fck already exists
[    1.073822] omap_i2c omap_i2c.3: bus 3 rev2.4.0 at 100 kHz
[    1.081146] registered am33xx_sr device
[    1.087554] mtdoops: mtd device (mtddev=name/number) must be supplied
[    1.094818] omap2-nand driver initializing
[    1.099304] OneNAND driver initializing
[    1.105102] CAN device driver interface
[    1.109130] CAN bus driver for Bosch D_CAN controller 1.0
[    1.124176] usb 1-1: New USB device found, idVendor=058f, idProduct=6254
[    1.131195] usb 1-1: New USB device strings: Mfr=0, Product=1, SerialNumber=0
[    1.138671] usb 1-1: Product: USB2.0Hub
[    1.143829] hub 1-1:1.0: USB hub found
[    1.147857] hub 1-1:1.0: 4 ports detected
[    1.163818] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[    1.170288] davinci_mdio davinci_mdio.0: detected phy mask fffffffe
[    1.177642] davinci_mdio.0: probed
[    1.181213] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver SMSC LAN8710/LAN8720
[    1.190216] usbcore: registered new interface driver zd1201
[    1.196289] usbcore: registered new interface driver cdc_ether
[    1.202606] usbcore: registered new interface driver cdc_eem
[    1.208740] usbcore: registered new interface driver dm9601
[    1.214630] cdc_ncm: 04-Aug-2011
[    1.218231] usbcore: registered new interface driver cdc_ncm
[    1.224182] Initializing USB Mass Storage driver...
[    1.229583] usbcore: registered new interface driver usb-storage
[    1.235900] USB Mass Storage support registered.
[    1.241302] mousedev: PS/2 mouse device common for all mice
[    1.248992] omap_rtc am33xx-rtc: rtc core: registered am33xx-rtc as rtc0
[    1.256103] am33xx-rtc: already running
[    1.260314] i2c /dev entries driver
[    1.264801] Linux video capture interface: v2.00
[    1.270019] usbcore: registered new interface driver uvcvideo
[    1.276062] USB Video Class driver (1.1.1)
[    1.284240] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[    1.367492] cpuidle: using governor ladder
[    1.372497] cpuidle: using governor menu
[    1.379302] omap4_aes_mod_init: loading AM33X AES driver
[    1.385009] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02
[    1.391876] omap4_aes_probe: probe() done
[    1.396667] omap4_sham_mod_init: loading AM33X SHA/MD5 driver
[    1.402832] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03
[    1.419738] omap4_sham_probe: probe() done
[    1.430633] usbcore: registered new interface driver usbhid
[    1.436523] usbhid: USB HID core driver
[    1.441589] usbcore: registered new interface driver snd-usb-audio
[    1.448760] usb 1-1.1: new low-speed USB device number 3 using musb-hdrc
[    1.458099] ALSA device list:
[    1.461212]   No soundcards found.
[    1.464813] oprofile: hardware counters not available
[    1.470092] oprofile: using timer interrupt.
[    1.474578] nf_conntrack version 0.5.0 (3952 buckets, 15808 max)
[    1.481536] ip_tables: (C) 2000-2006 Netfilter Core Team
[    1.487304] TCP cubic registered
[    1.490722] NET: Registered protocol family 17
[    1.495422] can: controller area network core (rev 20090105 abi 8)
[    1.502044] NET: Registered protocol family 29
[    1.506744] can: raw protocol (rev 20090105)
[    1.511230] can: broadcast manager protocol (rev 20090105 t)
[    1.517272] Registering the dns_resolver key type
[    1.522308] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[    1.530395] ThumbEE CPU extension supported.
[    1.534973] mux: Failed to setup hwmod io irq -22
[    1.540802] Power Management for AM33XX family
[    1.545776] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[    1.552490] Copied the M3 firmware to UMEM
[    1.556915] Cortex M3 Firmware Version = 0x18
[    1.561614] smartreflex smartreflex: am33xx_sr_probe: Zero NValue read from EFUSE
[    1.569488] smartreflex: probe of smartreflex failed with error -22
[    1.576873] sr_init: platform driver register failed
[    1.586700] clock: disabling unused clocks to save power
[    1.609252] mmc0: host does not support reading read-only switch. assuming write-enable.
[    1.619476] Detected MACID=0:18:31:93:55:15
[    1.625030] mmc0: new high speed SDHC card at address 1234
[    1.631591] cpsw: Detected MACID = 00:18:31:93:55:16
[    1.638397] mmcblk0: mmc0:1234 SA04G 3.67 GiB 
[    1.644836] omap_rtc am33xx-rtc: setting system clock to 2013-04-05 17:34:25 UTC (1365183265)
[    1.654602]  mmcblk0: p1 p2
[    1.663269] usb 1-1.1: New USB device found, idVendor=046d, idProduct=c05a
[    1.670562] usb 1-1.1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[    1.678283] usb 1-1.1: Product: USB Optical Mouse
[    1.683258] usb 1-1.1: Manufacturer: Logitech
[    1.691345] EXT3-fs (mmcblk0p2): recovery required on readonly filesystem
[    1.698547] EXT3-fs (mmcblk0p2): write access will be enabled during recovery
[    1.708007] input: Logitech USB Optical Mouse as /devices/platform/omap/musb-ti81xx/musb-hdrc.1/usb1/1-1/1-1.1/1-1.1:1.0/input/input0
[    1.721862] generic-usb 0003:046D:C05A.0001: input: USB HID v1.11 Mouse [Logitech USB Optical Mouse] on usb-musb-hdrc.1-1.1/input0
[    1.834106] usb 1-1.2: new low-speed USB device number 4 using musb-hdrc
[    1.961212] usb 1-1.2: New USB device found, idVendor=046d, idProduct=c31d
[    1.968566] usb 1-1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[    1.976257] usb 1-1.2: Product: USB Keyboard
[    1.980773] usb 1-1.2: Manufacturer: Logitech
[    1.996215] input: Logitech USB Keyboard as /devices/platform/omap/musb-ti81xx/musb-hdrc.1/usb1/1-1/1-1.2/1-1.2:1.0/input/input1
[    2.010192] generic-usb 0003:046D:C31D.0002: input: USB HID v1.10 Keyboard [Logitech USB Keyboard] on usb-musb-hdrc.1-1.2/input0
[    2.036224] input: Logitech USB Keyboard as /devices/platform/omap/musb-ti81xx/musb-hdrc.1/usb1/1-1/1-1.2/1-1.2:1.1/input/input2
[    2.049957] generic-usb 0003:046D:C31D.0003: input: USB HID v1.10 Device [Logitech USB Keyboard] on usb-musb-hdrc.1-1.2/input1
[    2.164550] usb 1-1.4: new high-speed USB device number 5 using musb-hdrc
[    2.286102] usb 1-1.4: New USB device found, idVendor=058f, idProduct=6366
[    2.293365] usb 1-1.4: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[    2.301086] usb 1-1.4: Product: Mass Storage Device
[    2.306243] usb 1-1.4: Manufacturer: Generic
[    2.310729] usb 1-1.4: SerialNumber: 058F0O1111B1
[    2.317443] scsi0 : usb-storage 1-1.4:1.0
[    3.315643] scsi 0:0:0:0: Direct-Access     Multi    Flash Reader     1.00 PQ: 0 ANSI: 0
[    3.329284] sd 0:0:0:0: [sda] Attached SCSI removable disk
[   12.247955] kjournald starting.  Commit interval 5 seconds
[   12.253845] EXT3-fs (mmcblk0p2): recovery complete
[   12.966674] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
[   12.973999] VFS: Mounted root (ext3 filesystem) readonly on device 179:2.
[   12.981658] Freeing init memory: 240K
INIT: version 2.88 booting
Starting udev
Error opening /dev/fb0: No such device
Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory
bootlogd.
[   16.833465] EXT3-fs (mmcblk0p2): using internal journal
ALSA: Restoring mixer settings...
Configuring network interfaces... /usr/sbin/alsactl: load_state:1686: No soundcards found...
[   17.503387] net eth0: CPSW phy found : id is : 0x7c0f1
udhcpc (v1.20.2) started
Sending discover...
Sending discover...
Sending discover...
No lease, failing
done.
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting Dropbear SSH server: dropbear.
Starting telnet daemon.
Performing wifi calibration...
rm: can't remove '/lib/firmware/ti-connectivity/wl1271-nvs.bin': No such file or directory
Error: Module wl12xx_sdio is not currently loaded
nl80211 not found.
[   27.242797] Disabling lock debugging due to kernel taint
Starting network benchmark server: netserver.
Starting syslogd/klogd: done
Starting thttpd.
Starting Lighttpd Web Server: lighttpd.
2013-04-05 17:34:51: (log.c.166) server started 
/
Starting Matrix GUI application.
[   46.283447]  gadget: Mass Storage Function, version: 2009/09/11
[   46.289825]  gadget: Number of LUNs=1
[   46.293701]  lun0: LUN: removable file: /dev/mmcblk0p1
[   46.299163]  gadget: Mass Storage Gadget, version: 2009/09/11
[   46.305206]  gadget: userspace failed to provide iSerialNumber
[   46.311401]  gadget: g_mass_storage ready
[   46.315643] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[   46.321289] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2
[   46.329254] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[   46.336425] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[   46.344024] usb usb2: Product: MUSB HDRC host driver
[   46.349273] usb usb2: Manufacturer: Linux 3.2.0 musb-hcd
[   46.354858] usb usb2: SerialNumber: musb-hdrc.0
[   46.360443] hub 2-0:1.0: USB hub found
[   46.364440] hub 2-0:1.0: 1 port detected
[   46.967987]  gadget: high-speed config #1: Linux File-Backed Storage
***************************************************************
***************************************************************
NOTICE: This file system contains the followin GPLv3 packages:
        binutils-symlinks
        binutils
        gdbserver
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution.  This can be done using
the opkg remove command.  i.e.:
    opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
      will be notified of the dependent packages.  You should
      use the --force-removal-of-dependent-packages option to
      also remove the dependent packages as well
***************************************************************
***************************************************************
Stopping Bootlog daemon: bootlogd.
 _____                    _____           _         _   
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_ 
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|  
              |___|                    |___|            
Arago Project http://arago-project.org am335x-evm ttyO0
Arago 2013.02 am335x-evm ttyO0
am335x-evm login: root
[   55.895996] usb 1-1.1: USB disconnect, device number 3
[   57.415618] usb 1-1.1: new low-speed USB device number 6 using musb-hdrc
[   57.539886] usb 1-1.1: New USB device found, idVendor=046d, idProduct=c05a
[   57.547180] usb 1-1.1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[   57.554870] usb 1-1.1: Product: USB Optical Mouse
[   57.559844] usb 1-1.1: Manufacturer: Logitech
[   57.580078] usb 1-1.1: can't set config #1, error -32
root@am335x-evm:~# 
Can anyone please suggest me something here, how to get out from this trouble.
Regards
Ram