This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PAndaboard OMAP 4460 flashing/Booting Android problem.

Hi,

        I followed steps from http://omappedia.org/wiki/4AJ.2.5_OMAP4-Panda_Jelly_Bean_Release_Notes to build android Jellybean 2.5 on Pandaboard ES. I am getting errors while booting. Even I have replaced ducati with recent one and recompiled it, but it was of no use, still I got the same error. My host is UBUNTU 12.04 64 bit. I have attached my log cat , please someone help me to solve this issue.

LOGCAT

shell@android:/ $ logcat  
--------- beginning of /dev/log/main
E/uim-sysfs(  103): uim: Inside main
E/uim-sysfs(  103): uim:ST built into the kernel ?
E/uim-sysfs(  103): uim:BT driver module un-available...  
E/uim-sysfs(  103): uim:BT driver built into the kernel ?
E/uim-sysfs(  103): uim:FM driver module un-available...  
E/uim-sysfs(  103): uim:FM driver built into the kernel ?
E/uim-sysfs(  103): uim:GPS driver module un-available...  
E/uim-sysfs(  103): uim:GPS driver built into the kernel ?
E/uim-sysfs(  103): uim:FM V4L2 driver module un-available...  
E/uim-sysfs(  103): uim:FM V4L2 driver built into the kernel ?
E/uim-sysfs(  103): uim:unable to chmod /dev/radio0, might not exist
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill0/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill1/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill2/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill3/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill4/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill5/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill6/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill7/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill8/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/clas[   43.835174] init: untracked pid 371 exited
s/rfkill/rfkill9/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill10/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill11/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill12/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill13/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill14/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill15/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill16/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill17/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill18/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill19/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill20/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill21/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill22/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill23/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill24/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill25/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill26/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill27/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill28/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill29/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill30/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill31/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill32/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill33/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill34/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill35/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill36/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill37/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill38/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill39/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill40/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
I/installd(  111): installd firing up
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill41/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill42/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill43/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill44/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill45/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill46/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill47/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill48/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/cutils  (  111): Failed to read /data/.layout_version: No such file or directory
E/uim-sysfs(  103): uim:open(/sys/class/rfkill/rfkill49/type) failed: No such file or directory (2)
E/uim-sysfs(  103):  
E/uim-sysfs(  103): uim:rfkill not enabled in st_drv - BT on from UI might fail
E/uim-sysfs(  103):  
D/installd(  111): Upgrading /data/media for multi-user
D/installd(  111): Upgrading to shared /data/media/obb
--------- beginning of /dev/log/system
I/Vold    (  100): Vold 2.1 (the revenge) firing up
D/Vold    (  100): Volume sdcard state changing -1 (Initializing) -> 0 (No-Media)
D/Vold    (  100): Volume usbflash1 state changing -1 (Initializing) -> 0 (No-Media)
D/Vold    (  100): Volume usbflash2 state changing -1 (Initializing) -> 0 (No-Media)
I/Netd    (  105): Netd 1.0 starting
W/InterfaceController(  105): Warning (Cannot load library: load_library(linker.cpp:745): library "/system/lib/libnetcmdiface.so" not found) while opening the net interface command library
I/DEBUG   (  106): debuggerd: Oct 22 2013 19:37:08
V/IMGSRV  (  101): Succesfully loaded gfx modules
I/SurfaceFlinger(  107): SurfaceFlinger is starting
I/SurfaceFlinger(  107): SurfaceFlinger's main thread ready to run. Initializing graphics H/W...
I/libEGL  (  107): Processor type: omap4460
I/libEGL  (  107): egl.cfg: entry POWERVR_SGX540_120 omap4430
I/libEGL  (  107): egl.cfg: entry POWERVR_SGX540_120 omap4460
I/libEGL  (  107): Picked EGL type 'POWERVR_SGX540_120' for processor 'omap4460'
D/libEGL  (  107): loaded /vendor/lib/egl/libEGL_POWERVR_SGX540_120.so
D/MDnsDS  (  105): MDnsSdListener::Hander starting up
D/MDnsDS  (  105): MDnsSdListener starting to monitor
D/MDnsDS  (  105): Going to poll with pollCount 1
D/libEGL  (  107): loaded /vendor/lib/egl/libGLESv1_CM_POWERVR_SGX540_120.so
D/libEGL  (  107): loaded /vendor/lib/egl/libGLESv2_POWERVR_SGX540_120.so
I/mediaserver(  110): ServiceManager: 0x409e3eb0
I/AudioFlinger(  110): Using default 3000 mSec as standby time.
I/CameraService(  110): CameraService started (pid=110)
D/DOMX    (  110): hardware/ti/domx/omx_core/src/OMX_Core.c:261    OMX_GetHandle()    
D/DOMX    (  110): ERROR: Can't open misc driver device 0xd
D/DOMX    (  110):  
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc.c:140    RPC_InstanceInit()    
D/DOMX    (  110): ERROR: Can't open device, errorno from open = 13
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc_stub.c:204    RPC_GetHandle()    
D/DOMX    (  110): ERROR: Write failed returning status = 0xffffffff
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc_stub.c:204    RPC_GetHandle()    
D/DOMX    (  110): ERROR: failed check:0 - returning error: 0x81001 - Write failed
D/DOMX    (  110): hardware/ti/domx/domx/omx_proxy_common/src/omx_proxy_common.c:2278    OMX_ProxyCommonInit()    
D/DOMX    (  110): ERROR: RPC function returned error 0x81001
D/DOMX    (  110): hardware/ti/domx/domx/omx_proxy_common/src/omx_proxy_common.c:2278    OMX_ProxyCommonInit()    
D/DOMX    (  110): ERROR: failed check:(eError == OMX_ErrorNone) - returning error: 0x80001001 - Error returned from OMX API in ducati
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc.c:261    RPC_InstanceDeInit()    
D/DOMX    (  110): ERROR: Close failed on omx fd
D/DOMX    (  110): hardware/ti/domx/omx_proxy_component/omx_camera/src/omx_proxy_camera.c:535    OMX_ComponentInit()    
D/DOMX    (  110): ERROR: rror in Initializing Proxy
E/CameraHal(  110): (400623dc)   hardware/ti/omap4xxx/camera/OMXCameraAdapter/OMXCameraAdapter.cpp:4276 OMXCameraGetHandle - OMX_GetHandle() failed, error: 0x80001001
W/libEGL  (  107): eglInitialize(0x1) failed (EGL_BAD_ALLOC)
D/DOMX    (  110): hardware/ti/domx/omx_core/src/OMX_Core.c:261    OMX_GetHandle()    
D/DOMX    (  110): ERROR: Can't open misc driver device 0xd
D/DOMX    (  110):  
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc.c:140    RPC_InstanceInit()    
D/DOMX    (  110): ERROR: Can't open device, errorno from open = 13
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc_stub.c:204    RPC_GetHandle()    
D/DOMX    (  110): ERROR: Write failed returning status = 0xffffffff
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc_stub.c:204    RPC_GetHandle()    
D/DOMX    (  110): ERROR: failed check:0 - returning error: 0x81001 - Write failed
D/DOMX    (  110): hardware/ti/domx/domx/omx_proxy_common/src/omx_proxy_common.c:2278    OMX_ProxyCommonInit()    
D/DOMX    (  110): ERROR: RPC function returned error 0x81001
D/DOMX    (  110): hardware/ti/domx/domx/omx_proxy_common/src/omx_proxy_common.c:2278    OMX_ProxyCommonInit()    
D/DOMX    (  110): ERROR: failed check:(eError == OMX_ErrorNone) - returning error: 0x80001001 - Error returned from OMX API in ducati
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc.c:261    RPC_InstanceDeInit()    
D/DOMX    (  110): ERROR: Close failed on omx fd
D/DOMX    (  110): hardware/ti/domx/omx_proxy_component/omx_camera/src/omx_proxy_camera.c:535    OMX_ComponentInit()    
D/DOMX    (  110): ERROR: rror in Initializing Proxy
E/CameraHal(  110): (400623dc)   hardware/ti/omap4xxx/camera/OMXCameraAdapter/OMXCameraAdapter.cpp:4276 OMXCameraGetHandle - OMX_GetHandle() failed, error: 0x80001001
D/DOMX    (  110): hardware/ti/domx/omx_core/src/OMX_Core.c:261    OMX_GetHandle()    
D/DOMX    (  110): ERROR: Can't open misc driver device 0xd
D/DOMX    (  110):  
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc.c:140    RPC_InstanceInit()    
D/DOMX    (  110): ERROR: Can't open device, errorno from open = 13
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc_stub.c:204    RPC_GetHandle()    
D/DOMX    (  110): ERROR: Write failed returning status = 0xffffffff
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc_stub.c:204    RPC_GetHandle()    
D/DOMX    (  110): ERROR: failed check:0 - returning error: 0x81001 - Write failed
D/DOMX    (  110): hardware/ti/domx/domx/omx_proxy_common/src/omx_proxy_common.c:2278    OMX_ProxyCommonInit()    
D/DOMX    (  110): ERROR: RPC function returned error 0x81001
D/DOMX    (  110): hardware/ti/domx/domx/omx_proxy_common/src/omx_proxy_common.c:2278    OMX_ProxyCommonInit()    
D/DOMX    (  110): ERROR: failed check:(eError == OMX_ErrorNone) - returning error: 0x80001001 - Error returned from OMX API in ducati
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc.c:261    RPC_InstanceDeInit()    
D/DOMX    (  110): ERROR: Close failed on omx fd
D/DOMX    (  110): hardware/ti/domx/omx_proxy_component/omx_camera/src/omx_proxy_camera.c:535    OMX_ComponentInit()    
D/DOMX    (  110): ERROR: rror in Initializing Proxy
E/CameraHal(  110): (400623dc)   hardware/ti/omap4xxx/camera/OMXCameraAdapter/OMXCameraAdapter.cpp:4276 OMXCameraGetHandle - OMX_GetHandle() failed, error: 0x80001001
D/DOMX    (  110): hardware/ti/domx/omx_core/src/OMX_Core.c:261    OMX_GetHandle()    
D/DOMX    (  110): ERROR: Can't open misc driver device 0xd
D/DOMX    (  110):  
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc.c:140    RPC_InstanceInit()    
D/DOMX    (  110): ERROR: Can't open device, errorno from open = 13
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc_stub.c:204    RPC_GetHandle()    
D/DOMX    (  110): ERROR: Write failed returning status = 0xffffffff
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc_stub.c:204    RPC_GetHandle()    
D/DOMX    (  110): ERROR: failed check:0 - returning error: 0x81001 - Write failed
D/DOMX    (  110): hardware/ti/domx/domx/omx_proxy_common/src/omx_proxy_common.c:2278    OMX_ProxyCommonInit()    
D/DOMX    (  110): ERROR: RPC function returned error 0x81001
D/DOMX    (  110): hardware/ti/domx/domx/omx_proxy_common/src/omx_proxy_common.c:2278    OMX_ProxyCommonInit()    
D/DOMX    (  110): ERROR: failed check:(eError == OMX_ErrorNone) - returning error: 0x80001001 - Error returned from OMX API in ducati
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc.c:261    RPC_InstanceDeInit()    
D/DOMX    (  110): ERROR: Close failed on omx fd
D/DOMX    (  110): hardware/ti/domx/omx_proxy_component/omx_camera/src/omx_proxy_camera.c:535    OMX_ComponentInit()    
D/DOMX    (  110): ERROR: rror in Initializing Proxy
E/CameraHal(  110): (400623dc)   hardware/ti/omap4xxx/camera/OMXCameraAdapter/OMXCameraAdapter.cpp:4276 OMXCameraGetHandle - OMX_GetHandle() failed, error: 0x80001001
D/DOMX    (  110): hardware/ti/domx/omx_core/src/OMX_Core.c:261    OMX_GetHandle()    
D/DOMX    (  110): ERROR: Can't open misc driver device 0xd
D/DOMX    (  110):  
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc.c:140    RPC_InstanceInit()    
D/DOMX    (  110): ERROR: Can't open device, errorno from open = 13
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc_stub.c:204    RPC_GetHandle()    
D/DOMX    (  110): ERROR: Write failed returning status = 0xffffffff
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc_stub.c:204    RPC_GetHandle()    
D/DOMX    (  110): ERROR: failed check:0 - returning error: 0x81001 - Write failed
D/DOMX    (  110): hardware/ti/domx/domx/omx_proxy_common/src/omx_proxy_common.c:2278    OMX_ProxyCommonInit()    
D/DOMX    (  110): ERROR: RPC function returned error 0x81001
D/DOMX    (  110): hardware/ti/domx/domx/omx_proxy_common/src/omx_proxy_common.c:2278    OMX_ProxyCommonInit()    
D/DOMX    (  110): ERROR: failed check:(eError == OMX_ErrorNone) - returning error: 0x80001001 - Error returned from OMX API in ducati
D/DOMX    (  110): hardware/ti/domx/domx/omx_rpc/src/omx_rpc.c:261    RPC_InstanceDeInit()    
D/DOMX    (  110): ERROR: Close failed on omx fd
D/DOMX    (  110): hardware/ti/domx/omx_proxy_component/omx_camera/src/omx_proxy_camera.c:535    OMX_ComponentInit()   

Thanks

cheluvaraj

  • Hello,

    First let me clarify that android is not supported on Pandaboard.

    Nevertheless have you tried the corresponding ducati pre-built  binary from http://omappedia.org/wiki/Android:_Working_with_pre-built_binaries? You may need to try both for Blaze & Blaze tablet.

    Best regards,

    Yordan