This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[OMAP3515] UART3 Configuration Question

I'm missing something.

I have a new, custom board featuring the 3515.  I am able to boot via UART3 and load u-boot.  When I load code in this manner, I can use my JTAG debugger and view UART3 address space at 0x49020000.  If I reset the board, load code via the JTAG and then execute, I get an access violation when I attempt to look at UART3 address space.  CM_ICLKEN_PER is set to 0x3ffff.  CM_FCLKEN_PER is set to 0x3ffff.  CM_AUTOIDLE_PER is zero. Other addresses in the L4 space (watchdog, gpio, etc.) are visible.  Obviously, I need to turn on something else.  I just don't know what I'm missing.

Any help will be appreciated.