Hi.
we are using two emacs in our NVR product. our env is DM8168 DVRRDK_04.00.00.03
GMAC0 - RTL8306M (HUB) phyid is 0~6
GMAC1 - RTL8211EG (LAN) phyid is 7
first we enable GMAC0, 4port HUB, it works
ifconfig eth0 192.168.1.33 up
PHY: 0:06 - Link is Up - 100/Full
second we enable GMAC1, LAN it not works.
net eth1: attached PHY driver [RTL8211E Gigabit Ethernet] (mii_bus:phy_addr=0:07, id=1cc915)
/mnt/usb1 # [rtl8211e_config_aneg]enter addr:0x7, mii_bus:d9eb3c00
PHY: 0:07 - Link is Up - 1000/Full
Because of this issue , i reboot the machine and only enable GMAC1 (disable GMAC 0) it works as follows.
/mnt/usb1 # ifconfig eth1 192.168.0.33 up
net eth1: attached PHY driver [RTL8211E Gigabit Ethernet] (mii_bus:phy_addr=0:07, id=1cc915)
/mnt/usb1 # [rtl8211e_config_aneg]enter addr:0x7, mii_bus:d9eb3c00
PHY: 0:07 - Link is Up - 100/Full
does anyone advice to me How to change Link up speed of GMAC1?
and any reference of use two GMAC?
i alreay read wiki , but it is not using two GMAC.
http://processors.wiki.ti.com/index.php?title=TI81XX_PSP_Ethernet_Switch_User_Guide#Bringing_Up_interfaces
Best Regards. CHO