This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Board validation for omap3430



HI,

Im new to OMAP platform.Is there some default board validation package provided for omap 3430.Any kind of cmm files etc.

 

Thank you

  • For the OMAP34xx you probably want to work with your local TI contacts for such support. From a OMAP35xx, at least in the case of the Mistral EVM board the board is validated through a software package known as ITBOK (Is The Board OK) that is included with the SDK install under OMAP35x_SDK_1.0.2\board_utilities\EVM3530_ITBOK, which is a set of software tests to verify the EVM hardware is functional, though I am not sure this is really the sort of board validation you are seeking as I am not very familiar with 'cmm files'.