Hi All,
could any body suggest me what should i do for this application...
i would like to make one application in which i am giving +15 volt DC voltage to any particular one pin of TMS320C5515 DSP Processor. when i give 15v dc then C5515 DSP Processor interrupt every things (whatever it is doing it should interrupt and it should give 1000Hz of Square wave to any pin of processor.
can any body suggest me what should i use in this application. because i can not use ADC hear .. in TMS320C5515 ADC take only max 1.5V input. so i can not use ADC hear. what should i go for ???
any idea ????
Please suggest me some code , library, or how can i solve this issue...
Thank in Advance...
Regard
Gaurav Garg