Other Parts Discussed in Thread: SYSBIOS
HI,Sir!
I want to use CLA-C as loop control, the process is:
1. select CPU timer(0,1or2), one of them , working as peroid and continuous mode, as ADC start trigger source
all ADC channel will be sample an converted by Sequence method.
2 start the cpu timer, and then it will start ADC sampling and converting
3. after all channel ADC result are ready, ADC module generate ADCINT1 interrupt
4. CLA task1 will be triggered by ADCINT1(of course, CLA task1 trigger by ADCINT1 mode)
I have a look some CLA-C demo project, such like iir2p2z, I have some question:
question A.
this CPU Timer for ADC starting trigger source, Does SYS BIOS need to deal CPU timer interrupt? if I disable CPU timer interrupt, can it trigger ADC sample and convert?
question B.
How to modify the following code that copied from iir2p2z_main.c for my SYSBIOS project? please see red code
The following is the original code
/* Assign user defined ISR to the PIE vector table */
EALLOW;
PieVectTable.CLA1_INT1 = &cla1_task1_isr;
PieVectTable.CLA1_INT2 = &cla1_task2_isr;
PieVectTable.CLA1_INT3 = &cla1_task3_isr;
PieVectTable.CLA1_INT4 = &cla1_task4_isr;
PieVectTable.CLA1_INT5 = &cla1_task5_isr;
PieVectTable.CLA1_INT6 = &cla1_task6_isr;
PieVectTable.CLA1_INT7 = &cla1_task7_isr;
PieVectTable.CLA1_INT8 = &cla1_task8_isr;
EDIS;
//Copy over the CLA code(if running in standalone mode from FLASH)
memcpy(&Cla1funcsRunStart, &Cla1funcsLoadStart, (Uint32)&Cla1funcsLoadSize);
//Copy over the CLA math tables(if running in standalone mode from FLASH
//and using the CLAMath Library)
//memcpy(&Cla1mathTablesRunStart, &Cla1mathTablesLoadStart, (Uint32)&Cla1mathTablesLoadSize);
/* Compute all CLA task vectors */
EALLOW;
Cla1Regs.MVECT1 = (Uint16)((Uint32)&Cla1Task1 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT2 = (Uint16)((Uint32)&Cla1Task2 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT3 = (Uint16)((Uint32)&Cla1Task3 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT4 = (Uint16)((Uint32)&Cla1Task4 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT5 = (Uint16)((Uint32)&Cla1Task5 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT6 = (Uint16)((Uint32)&Cla1Task6 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT7 = (Uint16)((Uint32)&Cla1Task7 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT8 = (Uint16)((Uint32)&Cla1Task8 -(Uint32)&Cla1Prog_Start);
EDIS;
// Step 3 : Mapping CLA tasks
/* All tasks are enabled and will be started by an ePWM trigger
* Map CLA program memory to the CLA and enable software breakpoints
*/
EALLOW;
Cla1Regs.MPISRCSEL1.bit.PERINT1SEL = CLA_INT1_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT2SEL = CLA_INT2_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT3SEL = CLA_INT3_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT4SEL = CLA_INT4_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT5SEL = CLA_INT5_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT6SEL = CLA_INT6_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT7SEL = CLA_INT7_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT8SEL = CLA_INT8_NONE;
Cla1Regs.MIER.all = 0x00FF;
EDIS;
/* Enable CLA interrupts at the group and subgroup levels */
PieCtrlRegs.PIEIER11.all = 0xFFFF;
IER = (M_INT11 );
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
/* Switch the CLA program space to the CLA and enable software forcing
* Also switch over CLA data ram 0,1 and 2
* CAUTION: The RAMxCPUE bits can only be enabled by writing to the register
* and not the individual bit field. Furthermore, the status of these bitfields
* is not reflected in either the watch or register views - they always read as
* zeros. This is a known bug and the user is advised to test CPU accessibilty
* first before proceeding
*/
EALLOW;
Cla1Regs.MMEMCFG.all = CLA_PROG_ENABLE|CLARAM0_ENABLE|CLARAM1_ENABLE|CLARAM2_ENABLE|CLA_RAM1CPUE;
Cla1Regs.MCTL.bit.IACKE = 1;
EDIS;
Tjhis is my code:
Because My code will start from flash memory.
/* Assign user defined ISR to the PIE vector table */
/* comment the following code ,because it shall be done by SYS BIOS, HWI ISR can be used
//EALLOW;
//PieVectTable.CLA1_INT1 = &cla1_task1_isr;
//PieVectTable.CLA1_INT2 = &cla1_task2_isr;
//PieVectTable.CLA1_INT3 = &cla1_task3_isr;
//PieVectTable.CLA1_INT4 = &cla1_task4_isr;
//PieVectTable.CLA1_INT5 = &cla1_task5_isr;
//PieVectTable.CLA1_INT6 = &cla1_task6_isr;
//PieVectTable.CLA1_INT7 = &cla1_task7_isr;
//PieVectTable.CLA1_INT8 = &cla1_task8_isr;
//EDIS;
/* un-comment memcpy code, because my code will start from flash memory
//Copy over the CLA code(if running in standalone mode from FLASH)
memcpy(&Cla1funcsRunStart, &Cla1funcsLoadStart, (Uint32)&Cla1funcsLoadSize);
//Copy over the CLA math tables(if running in standalone mode from FLASH
//and using the CLAMath Library)
memcpy(&Cla1mathTablesRunStart, &Cla1mathTablesLoadStart, (Uint32)&Cla1mathTablesLoadSize);
/* Compute all CLA task vectors */
EALLOW;
Cla1Regs.MVECT1 = (Uint16)((Uint32)&Cla1Task1 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT2 = (Uint16)((Uint32)&Cla1Task2 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT3 = (Uint16)((Uint32)&Cla1Task3 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT4 = (Uint16)((Uint32)&Cla1Task4 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT5 = (Uint16)((Uint32)&Cla1Task5 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT6 = (Uint16)((Uint32)&Cla1Task6 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT7 = (Uint16)((Uint32)&Cla1Task7 -(Uint32)&Cla1Prog_Start);
Cla1Regs.MVECT8 = (Uint16)((Uint32)&Cla1Task8 -(Uint32)&Cla1Prog_Start);
EDIS;
// Step 3 : Mapping CLA tasks
/* All tasks are enabled and will be started by an ePWM trigger
* Map CLA program memory to the CLA and enable software breakpoints
*/
EALLOW;
/* CLA TASK1 triggered by CLA_INT1_ADCINT1
Cla1Regs.MPISRCSEL1.bit.PERINT1SEL = CLA_INT1_ADCINT1;
Cla1Regs.MPISRCSEL1.bit.PERINT2SEL = CLA_INT2_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT3SEL = CLA_INT3_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT4SEL = CLA_INT4_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT5SEL = CLA_INT5_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT6SEL = CLA_INT6_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT7SEL = CLA_INT7_NONE;
Cla1Regs.MPISRCSEL1.bit.PERINT8SEL = CLA_INT8_NONE;
Cla1Regs.MIER.all = 0x00FF;
EDIS;
/* Enable CLA interrupts at the group and subgroup levels */
// shall be commented? because of SYS BIOS
/*
PieCtrlRegs.PIEIER11.all = 0xFFFF;
IER = (M_INT11 );
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
*/
/* Switch the CLA program space to the CLA and enable software forcing
* Also switch over CLA data ram 0,1 and 2
* CAUTION: The RAMxCPUE bits can only be enabled by writing to the register
* and not the individual bit field. Furthermore, the status of these bitfields
* is not reflected in either the watch or register views - they always read as
* zeros. This is a known bug and the user is advised to test CPU accessibilty
* first before proceeding
*/
EALLOW;
Cla1Regs.MMEMCFG.all = CLA_PROG_ENABLE|CLARAM0_ENABLE|CLARAM1_ENABLE|CLARAM2_ENABLE|CLA_RAM1CPUE;
Cla1Regs.MCTL.bit.IACKE = 1;
EDIS;