Hi,
I have questions about C6670 SPI Boot.
In our customer board, SPI NOR Flash Boot are used and the application only use L2RAM.
We don't use IBL so that it boots directly from NOR Flash.
But it looks like that boot is failing.
When I check the Program Counter from CCS after boot, it was stopping at 0x20B09A54.
This is Boot ROM area, so I guess the RBL is failing.
From CCS memory browser, DEVSTAT register was set to "0x0000140D"(SPI Boot mode)
and the BOOTCOMPLETE register was "all zero".
It seems that RBL reads only 80byte from NOR Flash.
What kind of thing is considered as a factor?
best regards,
g.f.