This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP-L137 Codec Server Build



I've continued with my attempts to build the server and am down to a list of warnings about "relocation type is static base-relative, but references symbol "_MBX_collect" defined in section ".mbx"; references to section ".mbx" are not relative to any static base, so this relocation cannot be performed (type = 'R_C60Base' (80), file = .../vqm_results.a674<vqm_results.obj>", offset = 0x00000480, section = ".text:algControl")

(The messages differ slightly, but they are all associated with calls to MBX_post.)

followed by

"warning: output file "vqm_results_server.x674" cannot be loaded and run on a target system"

followed by messages indicating that everything is up to date and complete.

What do the static base-relative messages mean?

Is there a synchonization method that will not run into the same problem?

Is the "cannot be loaded" message associated with the static base-relative message or is ist something else that I need to know about. They are all "warnings", not "errors", but that last one seems to suggest that I'm not getting anywhere.