Other Parts Discussed in Thread: OMAP-L137, OMAP-L138, AM1808
I have a few questions regarding JTAG debuggers and this seemed like the best thread to insert them.
We have a L137 EVM and are designing our own prototype board to use the L137 device.
Are the SD XDS510 emulators able to debug both cores? Independently and simultaneously?
Is there a preference among which emulator to use on the C6747 (Spectrum Digital vs. Blackhawk)?
If we want to do development/debug on just the ARM9, can we use the XDS 510 with an IDE other than CCS?
What would TI recommend as a development platform for the ARM9 (IDE and emulator)? What ARM9 emulators have been tested/verified on the L137?
Is it possible to plug in different emulators into each JTAG connector (20-pin and 14-pin) at the same time to perform independent debugging on separate IDEs (which may even be on separate PCs)?
Or is there a way to layout a design of the OMAP L137 so that each core (C6747 + ARM9) can have it's own JTAG? Maybe a better way to ask is this - does each core have a JTAG port or is there a single JTAG port that talks to both cores?
thanks,
Mike