The pin assignment application for the OMAP-L137 processor shows a conflict when using EMIFA and SD/MMC at the same time. EMIFA is required for NAND/NOR Flash. Curiously, the only conflict is data bus bits 0..3. This suggests that the problem could be mitigated by externally multiplexing the SD card onto the data bus. Is this in fact supported?
-Ted