Other Parts Discussed in Thread: AM5K2E02
Hello,
Does the security-accelator engine support VPN encryption? If so, than which features specifically (listed below) are required? If anyone has the specifics on this I would really appreciate it.
The features listed in the documentation for AM5K2E02/E04 are provided below for your reference:
› IPSec, SRTP, 3GPP and WiMAX Air Interface, and SSL/TLS Security
› ECB, CBC, CTR, F8, A5/3, CCM, GCM, HMAC, CMAC, GMAC, AES, DES, 3DES, Kasumi, SNOW 3G, SHA-1, SHA-2 (256-bit Hash), MD5
› Up To 6.4 Gbps IPSec and 3 Gbps Air Ciphering
Thanks,
Sean