This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[IPNC RDK 3.5] DM8127 UART1 u-boot

HI, all

We want use the uart1 as console. So I change the u-boot code

#define CONFIG_CONS_INDEX 1

to

#define CONFIG_CONS_INDEX 2

which in Source/ti_tools/ipnc_psp_arago/u-boot/include/configs/ti8148_ipnc.h

I recompile it and flashed u-boot.min.nand. But it does not work.

Any other places should I change?

pls give me some suggestions. Thank you.

  • Hi Haitao,

    I am working only on DM814x EZSDK, so I can only provide you the below wiki page for reference, it might be in help:

    http://processors.wiki.ti.com/index.php/TI81xx_PSP_Porting_Guide#Using_different_UART_than_the_default_EVM_configuration_as_console

    I will notify our DM8127 IPNC team for help.

    Regards,
    Pavel