Other Parts Discussed in Thread: OMAP3530
I have built and run the DVSDK demo applications, but needed to modify the CMEM settings before it would work.
The intital cmem settings were loaded from the /opt/dvsdk/loadmodules.sh file:
insmod cmemk.ko phys_start=0x85800000 phys_end=0x86800000 pools=20x4096,8x131072,5x1048576,1x1429440,1x256000,1x3600000,5x829440
and this allows the default demo interface and decode applications to startup and run fine. However the audio_copy and video_copy applications produce the following error with these settings:
[root@OMAP3EVM video_copy]# ./app.out
App-> Application started.
Configuration error: Exceeded maximum number [31] of Translation Look-aside Buf
fers.
@0x00069a07:[T:0x40964490] OP - Processor_create_d> Loading and starting DSP ser
ver 'video_copy.x64P' FAILED, status=[0x80008052] (look for error code 'DSP_EBAS
E + 0x52' in dsplink*/packages/dsplink/gpp/inc/errbase.h)
@0x00069b1a:[T:0x40964490] OP - Processor_delete_d> Closing remote transport FAI
LED, status=0x80008002.
@0x00069b57:[T:0x40964490] OP - Processor_delete_d> Stopping DSP FAILED, status=
0x80008002
@0x00069b94:[T:0x40964490] OP - Processor_delete_d> Closing pool FAILED, status=
0x80008000
@0x00069bb2:[T:0x40964490] OP - Processor_delete_d> Detaching from DSP FAILED, s
tatus=0x80008000
@0x0006df4a:[T:0x4001cfb0] CE - rserverOpen: can't start 'video_copy.x64P'; Proc
essor_create failed
CEapp-> ERROR: can't open engine video_copy
App-> Application FAILED.
[root@OMAP3EVM video_copy]#
So modifing the cmem to this:
insmod cmemk.ko phys_start=0x85800000 phys_end=0x86000000 pools=20x4096,10x131072,2x1048576
now the video_copy app runs fine, but then produces similar Configuration buffer errors with the original interface and decode demo application.
It would appear the different applications are configured for aquiring different memory pools. And the cmem configurations are not compatilble for each of the different applications.
So the questions I have are:
1. where is the memory configured for each of the applications? (.tcf or .tci files)
2. How are the cmem initialization configuration related to the application configuration memory requirements?
Thanks for any help.
-simon