Hi. I hope im in the right forum.
Im running the WinCe "S1SDKOMAP_DVSDK_OMAPWINCE_EA_06_10_00"
Copyed from /BSP/readme.txt
<5/2/08 6.00.00>
- Initial Release
***********************************
Known Hardware Issues
***********************************
- The EVM DB9 UART1/2 and UART3 serial ports only support RXD and TXD,
there are no modem handshake signals available.
Is this still the case? running 6.09 now and read thru the 6.10 changes.
I need to check the Clear to send flag. Is this possible in 6.09/6.10?
Im using Uart1.
//Jonas