Hi ,
I am using Beagle Board and Angstrom Filesystem . Angstrom Filesystem is compatible for 2.6.28 kernel , they have supplied , encodeCombo.x264P and decodeCombo.x264P as well as video_encode_io1_omap3530.x470MV and video_decode_io2_omap3530.x470MV which are working properly. It looks like dvsdk 3_00_00_29 which is working on Mistral OMAP3530 board with kernel 2.6.22.18 supplied by TI but if I take these codec Engine combos and sample app then nothing is working on Beagle Board and giving the error as Failed to determine the target board. I want to compile dvsdk 3_00_00_29 for Beagle Board. How is it possible? Can I use the sample app for Mistral on BeagleBoard?
It looks OE provides Gstreamer to access the cmemk,dsplink to encode and decode video. However I got gstreamer supplied by TI but how to link it with dvsdk_3__00__00__29 and how to compile. How does gstreamer helps in encode, decode and display on display monitor connected with Beagle Board.
Regards, Vineet