Other Parts Discussed in Thread: OMAP-L137
Hi,
I am planning to use OMAP L137 based platform (EVMOMAPL137) In my project. I learnt from internet that GA-SDK release of the stack (and its previous version) will have USB driver included.
My question is related to USB. If I want to configure my device as USB mass storage device and also compatible to printer class device(USB OTG functionality) what will be the effort for application development when I use the GA SDK driver stack? Does it include some sample code for USB OTG device and host? Can you comment on the complexity?
One more question on the LCD driver: It is a 16 bit LCD controller, can you indicate some of the compatible LCD display devices that it can connect to?
Regards.